Reads the results of A/D conversion.
[Syntax]
#include “r_cg_macrodriver.h”
void R_PGA_DSAD_Get_Result ( uint16_t * const bufferH, uint16_t * const bufferL );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       uint16_t * const bufferH;  | 
    
       Pointer to area in which to store the results of A/D conversion (DSADCRM resister and DSADCRH resister)  | 
| 
       O  | 
    
       uint16_t * const bufferLl;  | 
    
       Pointer to area in which to store the results of A/D conversion (DSADCRC resister and DSADCRL resister)  | 
[Return value]
None.