Starts the alarm interrupt function.(in the case of the calendar mode setting)
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
void R_RTC_Set_CalendarAlarmOn ( uint8_t enb_set );
[Argument(s)]
| I/O | Argument | Description | 
| I | uint8_t enb_set; | Alarm enable | 
Remark Below is shown the structure enb_set.
|  | 
[Return value]
None.