Everything
1.4 License

A license manager manages licenses to the compilers.

If you have a license, the compiler will operate as the Standard or Professional edition depending on the license you are using.

Refer to "1.5 Standard and Professional Editions" for more on the Standard and Professional editions.

If the license manager is not able to recognize a Standard or Professional license, the compiler operates as the free evaluation edition.

Refer to "1.6 Free Evaluation Editions" for more on the free evaluation edition.

For details of the licenses and the license manager, refer to the User's Manual of the License Manager.

Use V2.00 or later versions of the license manager for V1.05 and later versions of CC-RH.

Use a license for V2 or later versions of CC-RH in development for the RH850 G4 core.