Everything

 

-Xmisra2012 [Professional Edition only]


This option checks source code against the MISRA-C:2012 rules.

[Specification format]

-Xmisra2012=item[=value]

 

-

Interpretation when omitted

The source code is not checked against the MISRA-C:2012 rules.

[Detailed description]

-

This option checks source code against the MISRA-C:2012 rules.
A message is output if the item specified for the check is item.

-

This option cannot be specified simultaneously with the -Xmisra2004 option.

-

The items that can be specified as item are shown below.
An error will occur if any other item is specified.
The source code is always checked against the rules of the "mandatory" type regardless of the following specification.

Check Item (item)

Parameter (value)

Description

all

None

The source code is checked against all of the rules which are supported.

apply

num[,num]...

The source code is checked against the rules with the numbers specified by num among the rules which are supported.

ignore

num[,num]...

The source code is checked against the rules with the numbers that are not specified by num among the rules which are supported.

required

None

The source code is checked against the rules of the "mandatory" and "required" types among the rules which are supported.

required_add

num[,num]...

The source code is checked against the rules of the "mandatory" and "required" types and the rules with the numbers specified by num among the rules which are supported.

required_remove

num[,num]...

The source code is checked against the rules of the "required" type except for the rules with the numbers specified by num among the rules which are supported.

file

The source code is checked against the rules with the numbers described in specified file file among the rules which are supported.

Specify one rule number per one line in the file.

 

-

In V2.02.00 or later, the following rule numbers are supported based on MISRA-C:2012 Amendment 1.

An error will occur if any other item is specified.

2.2 2.6 2.7

3.1 3.2

4.1 4.2

5.1 5.2 5.3 5.4 5.5 5.6 5.7 5.8 5.9

6.1 6.2

7.1 7.2 7.3 7.4

8.1 8.2 8.3 8.4 8.5 8.6 8.8 8.9 8.11 8.12 8.13 8.14

9.1 9.2 9.3 9.4 9.5

10.1 10.2 10.3 10.4 10.5 10.6 10.7 10.8

11.1 11.2 11.3 11.4 11.5 11.6 11.7 11.8 11.9

12.1 12.2 12.3 12.4 12.5

13.1 13.2 13.3 13.4 13.5 13.6

14.2 14.3 14.4

15.1 15.2 15.3 15.4 15.5 15.6 15.7

16.1 16.2 16.3 16.4 16.5 16.6 16.7

17.1 17.3 17.4 17.5 17.6 17.7 17.8

18.4 18.5 18.7

19.2

20.1 20.2 20.3 20.4 20.5 20.6 20.7 20.8 20.9 20.10 20.11 20.12 20.13 20.14

21.1 21.2 21.3 21.4 21.5 21.6 21.7 21.8 21.9 21.10 21.11 21.12 21.13 21.15 21.16

-

An error will occur if item is omitted.

-

The __fp16 type is handled as the float type during the check. For the effects of this handling, see the description of the -Xcheck_language_extension [Professional Edition only] option.

[Example of use]

-

To check the source code against MISRA-C:2012 rule number: 5.2, 5.3, and 5.4, describe as:

>ccrh -Xmisra2012=apply=5.2,5.3,5.4 -Xcommon=rh850 main.c