Everything

 

-Xfloat


This option controls generating floating-point calculation instructions.

[Specification format]

-Xfloat=type

 

-

Interpretation when omitted

If the-Xcpu=g3k option is specified, -Xfloat=soft is assumed.

In any other case, -Xfloat=fpu is assumed.

[Detailed description]

-

This option controls generating floating-point calculation instructions.

-

The items that can be specified as type are shown below.
An error will occur if any other item is specified.

soft

Generates runtime function call instructions for floating-point calculations.

fpu

Generates floating-point calculation instructions of FPU (floating-point unit) for floating-point calculations.

However, if -Xcpu=g3kh is specified, runtime function call instructions for double-precision calculations will be generated.

If this option is specified together with the -Xcpu=g3k option, this option is invalid and -Xfloat=soft is assumed.

 

-

An error will occur if type is omitted.

-

If soft is specified as type, the -Xround=zero option will be invalid and -Xround=nearest will always be valid.

-

If the specification of this option is changed for each source file, registers may not be correctly managed in exception handlers.

[Example of use]

-

To generate the jarl32 and jr32 instructions for function-call branches, describe as:

>ccrh -Xfloat=soft -Xcommon=rh850 main.c