7.5.2 Character operation functions
Character operation functions are as follows.
Table 7.4 | Character operation Functions |
|
|
|
|
isalnum
|
Identification of ASCII letter or numeral
|
|
isalpha
|
Identification of ASCII letter
|
|
isascii
|
Identification of ASCII code
|
|
isblank [V1.07 or later]
|
Identification of space or tab (C99)
|
|
iscntrl
|
Identification of control character
|
|
isdigit
|
Identification of decimal number
|
|
isgraph
|
Identification of display character other than space
|
|
islower
|
Identification of lower-case character
|
|
isprint
|
Identification of display character
|
|
ispunct
|
Identification of delimiter character
|
|
isspace
|
Identification of space/tab/carriage return/line feed/vertical tab/page feed
|
|
isupper
|
Identification of upper-case character
|
|
isxdigit
|
Identification of hexadecimal number
|
|
toascii
|
Judges if a character is an ASCII code
|
|
tolower
|
Conversion from upper-case to lower-case (not converted if argument is not in upper-case)
|
|
toupper
|
Conversion from lower-case to upper-case (not converted if argument is not in lower-case)
|