< Compile Options / Object Options >
The default for this option is -stuff.
When the nostuff option is specified, the compiler allocates the variables belonging to the specified <section type> to 4-byte boundary alignment sections. When <section type> is omitted, variables of all section types are applicable. |
C, D, and B are the section names specified by the section option or #pragma section. W is the section name specified by the section option. The data contents allocated to each section are output in the order they were defined. |