< Compile Options / Other Options >
The static analysis information file is not output.
This option specifies the location where the static analysis information file to be generated during compilation as path. |
If an existing folder is specified as path, the static analysis information file is saved under the C source file name with the extension replaced by .cref to path. |
If an existing file name is specified or a non-existing folder or file name is specified, the static analysis information file is output with path as the file name when one static analysis information file is output. |
If two or more files with the same name (even if they are in different folders) are specified as source files, then a warning is output, and a static analysis information file is only saved for the last source file to be specified. |
To output the static analysis information file as file name info.cref, describe as: