Everything
4.1.7 Conforming Language Specifications

(1)

C Language Specifications (When the lang=c Option is Selected)

ANSI/ISO 9899-1990 American National Standard for Programming Languages -C

(2)

C Language Specifications (When the lang=c99 Option is Selected)

ISO/IEC 9899:1999 INTERNATIONAL STANDARD Programming Languages - C

However, variable length arrays are excluded.

(3)

C++ Language Specifications (When the lang=cpp Option is Selected)

Based on the language specifications compatible with Microsoft® Visual C/C++ 6.0