The following extended specifications can also be used with the _Pragma operator in C99.
This extension changes the section name to be output by the compiler.
For details on the description, refer to (1) Section Switch.
This extension creates the stack section.
For details on the description, refer to (2) Stack Section Creation.
This extension creates the interrupt function.
For details on the description, refer to (3) Interrupt Function Creation.
This extension expands a function.
For details on the description, refer to (4) Inline Expansion of Function.
This extension cancels expansion of a function.
For details on the description, refer to (4) Inline Expansion of Function.
This extension creates the assembly-language inline functions.
For details on the description, refer to (5) Inline Expansion of Assembly-Language Function.
This extension specifies the entry function.
For details on the description, refer to (6) Entry Function Specification.
This extension specifies the order of the bit field.
For details on the description, refer to (7) Bit Field Order Specification.
This extension specifies the boundary alignment value of structure members and class members as 1 byte.
For details on the description, refer to (8) Alignment Value Specification for Structure Members and Class Members.
This extension specifies the boundary alignment value for structure members and class members as the value for members.
For details on the description, refer to (8) Alignment Value Specification for Structure Members and Class Members.
This extension specifies the option of the boundary alignment value for structure members and class members.
For details on the description, refer to (8) Alignment Value Specification for Structure Members and Class Members.
This extension allocates the specified variable to the specified address.
For details on the description, refer to (9) Allocation of a Variable to the Absolute Address.
This extension specifies an endian for initial values.
For details on the description, refer to (10) Endian Specification for Initial Values.
Specification of Function in which Instructions at Branch Destinations are Aligned to 4-Byte Boundaries |
This extension specifies the function in which instructions at branch destinations are aligned to 4-byte boundaries.
For details on the description, refer to (11) Specification of Function in which Instructions at Branch Destinations are Aligned for Execution.
Specification of Function in which Instructions at Branch Destinations are Aligned to 8-Byte Boundaries |
This extension specifies the function in which instructions at branch destinations are aligned to 8-byte boundaries.
For details on the description, refer to (11) Specification of Function in which Instructions at Branch Destinations are Aligned for Execution.
This extension specifies the function in which instructions at branch destinations are not aligned.
For details on the description, refer to (11) Specification of Function in which Instructions at Branch Destinations are Aligned for Execution.
Specification of Function for generating a code for detection of stack smashing [Professional Edition only] [V2.04.00 or later] |
This extension generates a code for detection of stack smashing.
For details on the description, refer to (12) Specification of Function for generating a code for detection of stack smashing [Professional Edition only] [V2.04.00 or later].
Specification of not generating a code for detection of stack smashing [Professional Edition only] [V2.04.00 or later] |
This extension suppress generating generate a code for detection of stack smashing.
For details on the description, refer to (12) Specification of Function for generating a code for detection of stack smashing [Professional Edition only] [V2.04.00 or later].