Instructions are translated into object codes (machine language) as a result of assembling, but directives are not converted into object codes in principle.
Directives contain the following functions mainly:
- | To facilitate description of source programs |
- | To initialize memory and reserve memory areas |
- | To provide the information required for assemblers and linkers to perform their intended processing |
The following table shows the types of directives.
|
|
Link directives
|
.SECTION, .GLB, .WEAK [V3.07 or later], .RVECTOR
|
Assembler directives
|
.EQU, .END, .INCLUDE
|
Address directives
|
.ORG, .OFFSET, .ENDIAN, .BLKB, .BLKW, .BLKL, .BLKD, .BYTE, .WORD, .LWORD, .FLOAT, .DOUBLE, .ALIGN
|
Macro directives
|
.MACRO, .EXITM, .LOCAL, .ENDM, .MREPEAT, .ENDR, ..MACPARA, ..MACREP, .LEN, .INSTR, .SUBSTR
|
Specific compiler directives
|
._LINE_TOP, ._LINE_END, .SWSECTION, .SWMOV, .SWITCH, .INSTALIGN
|
The following sections explain the details of each directive.