Everything
7.4.7 <math.h>

Performs various mathematical operations.

The following constants (macros) are all implementation-defined.

Type

Definition Name

Description

Constant
(macro)

EDOM

Indicates the value to be set in errno if the value of a parameter input to a function is outside the range of values defined in the function.

ERANGE

Indicates the value to be set in errno if the result of a function cannot be represented as a double type value, or if an overflow or an underflow occurs.

HUGE_VAL

HUGE_VALF <-lang=c99>

HUGE_VALL <-lang=c99>

Indicates the value for the function return value if the result of a function overflows.

INFINITY <-lang=c99>

Expanded to a float-type constant expression that represents positive or unsigned infinity.

NAN <-lang=c99>

Defined when float-type qNaN is supported.

FP_INFINITE <-lang=c99>

FP_NAN <-lang=c99>

FP_NORMAL <-lang=c99>

FP_SUBNORMAL <-lang=c99>

FP_ZERO <-lang=c99>

These indicate exclusive types of floating-point values.

FP_ILOGB0 <-lang=c99>

FP_ILOGBNAN <-lang=c99>

These are expanded to an integer constant expression of the value returned by ilogb when they are 0 or not-a-number, respectively.

MATH_ERRNO <-lang=c99>

MATH_ERREXCEPT <-lang=c99>

These are expanded to integer constants 1 and 2, respectively.

math_errhandling <-lang=c99>

Expanded to an int-type expression whose value is a bitwise logical OR of MATH_ERRNO and MATH_ERREXCEPT.

Type

float_t <-lang=c99>

double_t <-lang=c99>

These are floating-point types having the same width as float and double, respectively.

Function (macro)

fpclassify <-lang=c99>

Classifies argument values into not-a-number, infinity, normalized number, denormalized number, and 0.

isfinite <-lang=c99>

Determines whether the argument is a finite value.

isinf <-lang=c99>

Determines whether the argument is infinity.

isnan <-lang=c99>

Determines whether the argument is a not-a-number.

isnormal <-lang=c99>

Determines whether the argument is a normalized number.

signbit <-lang=c99>

Determines whether the sign of the argument is negative.

isgreater <-lang=c99>

Determines whether the first argument is greater than the second argument.

isgreaterequal <-lang=c99>

Determines whether the first argument is equal to or greater than the second argument.

isless <-lang=c99>

Determines whether the first argument is smaller than the second argument.

islessequal <-lang=c99>

Determines whether the first argument is equal to or smaller than the second argument.

islessgreater <-lang=c99>

Determines whether the first argument is smaller or greater than the second argument.

isunordered <-lang=c99>

Determines whether the arguments are not ordered.

Function

acos / acosf / acosl

Calculates the arc cosine of a floating-point number.

asin / asinf / asinl

Calculates the arc sine of a floating-point number.

atan / atanf / atanl

Calculates the arc tangent of a floating-point number.

atan2 / atan2f / atan2l

Calculates the arc tangent of the result of a division of two floating-point numbers.

cos / cosf / cosl

Calculates the cosine of a floating-point radian value.

sin / sinf / sinl

Calculates the sine of a floating-point radian value.

tan / tanf / tanl

Calculates the tangent of a floating-point radian value.

cosh / coshf / coshl

Calculates the hyperbolic cosine of a floating-point number.

sinh / sinhf / sinhl

Calculates the hyperbolic sine of a floating-point number.

tanh / tanhf / tanhl

Calculates the hyperbolic tangent of a floating-point number.

exp / expf / expl

Calculates the exponential function of a floating-point number.

frexp / frexpf / frexpl

Breaks a floating-point number into a [0.5, 1.0) value and a power of 2.

ldexp / ldexpf / ldexpl

Multiplies a floating-point number by a power of 2.

log / logf / logl

Calculates the natural logarithm of a floating-point number.

log10 / log10f / log10l

Calculates the base-ten logarithm of a floating-point number.

modf / modff / modfl

Breaks a floating-point number into integral and fractional parts.

pow / powf / powl

Calculates a power of a floating-point number.

sqrt / sqrtf / sqrtl

Calculates the positive square root of a floating-point number.

Function

ceil / ceilf / ceill

Calculates the smallest integral value not less than or equal to the given floating-point number.

fabs / fabsf / fabsl

Calculates the absolute value of a floating-point number.

floor / floorf / floorl

Calculates the largest integral value not greater than or equal to the given floating-point number.

fmod / fmodf / fmodl

Calculates the remainder of a division of two floating-point numbers.

acosh / acoshf / acoshl

<-lang=c99>

Calculates the hyperbolic arc cosine of a floating-point number.

asinh / asinhf / asinhl

<-lang=c99>

Calculates the hyperbolic arc sine of a floating-point number.

atanh / atanhf / atanhl

<-lang=c99>

Calculates the hyperbolic arc tangent of a floating-point number.

exp2 / exp2f / exp2l

<-lang=c99>

Calculates the value of 2 raised to the power x.

expm1 / expm1f / expm1l

<-lang=c99>

Calculates the natural logarithm raised to the power x and subtracts 1 from the result.

ilogb / ilogbf / ilogbl

<-lang=c99>

Extracts the exponent of x as a signed int value.

log1p / log1pf / log1pl

<-lang=c99>

Calculates the natural logarithm of the argument + 1.

log2 / log2f / log2l

<-lang=c99>

Calculates the base-2 logarithm.

logb / logbf / logbl

<-lang=c99>

Extracts the exponent of x as a signed integer.

scalbn / scalbnf / scalbnl / scalbln / scalblnf / scalblnl

<-lang=c99>

Calculates x × FLT_RADIXn.

cbrt / cbrtf / cbrtl

<-lang=c99>

Calculates the cube root of a floating-point number.

hypot / hypotf / hypotl

<-lang=c99>

Calculates the square root of the sum of squares of two

 

parameters ( ).

erf / erff / erfl

<-lang=c99>

Calculates the error function.

erfc / erfcf / erfcl

<-lang=c99>

Calculates the complementary error function.

lgamma / lgammaf / lgammal

<-lang=c99>

Calculates the natural logarithm of the absolute value of the gamma function.

tgamma / tgammaf / tgammal

<-lang=c99>

Calculates the gamma function.

nearbyint / nearbyintf / nearbyintl

<-lang=c99>

Rounds a floating-point number to an integer in the floating-point representation according to the current rounding direction.

rint / rintf / rintl

<-lang=c99>

Equivalent to nearbyint except that this function group may generate floating-point exception.

Function

lrint / lrintf / lrintl / llrint / llrintf / llrintl

<-lang=c99>

Rounds a floating-point number to the nearest integer according to the rounding direction.

round / roundf / roundl

<-lang=c99>

Rounds a floating-point number to the nearest integer in the floating-point representation.

lround / lroundf / lroundl / llround / llroundf / llroundl

<-lang=c99>

Rounds a floating-point number to the nearest integer.

trunc / truncf / truncl

<-lang=c99>

Rounds a floating-point number to the nearest integer in the floating-point representation.

remainder / remainderf / remainderl

<-lang=c99>

Calculates remainder x REM y specified in the IEEE60559 standard.

remquo / remquof / remquol

<-lang=c99>

Calculates the value having the same sign as x/y and the absolute value congruent modulo-2n to the absolute value of the quotient.

copysign / copysignf / copysignl

<-lang=c99>

Generates a value consisting of the given absolute value and sign.

nan / nanf / nanl

<-lang=c99>

nan("n string") is equivalent to ("NAN(n string)", (char**) NULL).

nextafter / nextafterf / nextafterl

<-lang=c99>

Converts a floating-point number to the type of the function and calculates the representable value following the converted number on the real axis.

nexttoward / nexttowardf / nexttowardl

<-lang=c99>

Equivalent to the nextafter function group except that the second argument is of type long double and returns the second argument after conversion to the type of the function.

fdim / fdimf / fdiml

<-lang=c99>

Calculates the positive difference.

fmax / fmaxf / fmaxl

<-lang=c99>

Obtains the greater of two values.

fmin / fminf / fminl

<-lang=c99>

Obtains the smaller of two values.

fma / fmaf / fmal

<-lang=c99>

Calculates (d1 * d2) + d3 as a single ternary operation.

 

Operation in the event of an error is described below.

(1)

Domain error

A domain error occurs if the value of a parameter input to a function is outside the domain over which the mathematical function is defined. In this case, the value of EDOM is set in errno. The function return value in implementation-defined.

(2)

Range error

A range error occurs if the result of a function cannot be represented as a value of the double type. In this case, the value of ERANGE is set in errno. If the result overflows, the function returns the value of HUGE_VAL, HUGE_VALF, or HUGE_VALL with the same sign as the correct value of the function. If the result underflows, 0 is returned as the return value.

Notes 1.

If there is a possibility of a domain error resulting from a <math.h> function call, it is dangerous to use the resultant value directly. The value of errno should always be checked before using the result in such cases.

[Format]

              .
              .
              .
         1   x=asin(a);
         2   if (errno==EDOM)
         3       printf ("error\n");
         4   else
         5       printf ("result is : %lf\n",x);
              .
              .
              .

 

In line 1, the arc sine value is computed using the asin function. If the value of argument a is outside the asin function domain [–1.0, 1.0], the EDOM value is set in errno. Line 2 determines whether a domain error has occurred. If a domain error has occurred, error is output in line 3. If there is no domain error, the arc sine value is output in line 5.

Notes 2.

Whether or not a range error occurs depends on the internal representation format of floating-point types determined by the compiler. For example, if an internal representation format that allows an infinity to be represented as a value is used, <math.h> library functions can be implemented without causing range errors.

 

Implementation-Defined Specifications

Item

Compiler Specifications

Value returned by a mathematical function if an input argument is out of the range

A not-a-number is returned. For details on the format of not-a-numbers, refer to section "(5) Floating-Point Number Specifications" in "4.1.5 Internal Data Representation and Areas".

Whether errno is set to the value of macro ERANGE if an underflow error occurs in a mathematical function

For the functions that set errno to the value of ERANGE, see "10.5.6 Standard Library Error Messages". The other functions do not set errno to ERANGE.

Whether a range error occurs if the second argument in the fmod function is 0

A range error occurs.

For details of the return value from fmod, see "fmod / fmodf / fmodl" in "7.4.7 <math.h>".