9.2.2
Referencing C/C++ Program External Names (Variables and C Functions)
from Assembly-Language Programs
A C/C++ program can define external variable names (without an underscore (_)).
In an assembly-language program, .GLB is used to declare an external name (preceded by an underscore).
[Example of C source]
[Example of assembly-language source]
.GLB _a
.SECTION P,CODE
MOV.L #A_a,R1
MOV.L [R1],R2
ADD #1,R2
MOV.L R2,[R1]
RTS
.SECTION D,ROMDATA,ALIGN=4
A_a: .LWORD _a
.END
|