This dialog box is used to set the scroll range of the vertical scroll bar on the Memory panel/Disassemble panel.
By setting the appropriate range, it is possible to improve the operability of a mouse (e.g. dragging) because the size of the vertical scroll bar on the panel is changed suitably.
After setting a scroll range via this dialog box, the scroll range is not updated automatically even if the address evaluated by the address expression is changed because of such as a line assembly.  | 
It is possible to move outside the scroll range by using the [Page Up]/[Page Down]/[Up]/[Down] key, a button at either end of the scroll bar or a menu item related to the jump function.  | 
This section describes the following.
On the Memory panel, click the   | 
On the Memory panel, select the [View] menu >> [Settings Scroll Range...] from the context menu.  | 
On the Disassemble panel, click the   | 
On the Disassemble panel, select the [View] menu >> [Settings Scroll Range...] from the context menu.  | 
Specify the start address of the range of scrolling.
You can either type an address expression directly into the text box (up to 1024 characters), or select it from the input history via the drop-down list (up to 10 items).
Note that the setting of the scroll range is not performed if "All" is selected in the drop-down list at this time (the scroll range is not limited).
A symbol name at the current caret position can be complemented by pressing the [Ctrl] + [Space] key in this text box (see "2.20.2 Symbol name completion function").  | 
Specify the end address of the range of scrolling.
You can either type an address expression directly into the text box (up to 1024 characters), or select it from the input history via the drop-down list (up to 10 items).
Note that this area becomes invalid if [Start address] is specified with [All].
A symbol name at the current caret position can be complemented by pressing the [Ctrl] + [Space] key in this text box (see "2.20.2 Symbol name completion function").  | 
 button from [View] on the toolbar.
 button from [View] on the toolbar.