Contents of the SFR can be displayed and its values can be changed in the SFR panel below.
Select the [View] menu >> [SFR].
For details on the contents and function in each area, see the section for the SFR panel.

This section describes the following.
2.10.3.3 Change display format of values
2.10.3.5 Display/modify the SFR contents during program execution
2.10.3.5 Display/modify the SFR contents during program execution