To reset CPU, click the
button on the debug toolbar.
When CPU is reset, the current PC value is set to the reset address.
You can automatically overwrite the value of SFR/CPU register with the specified values after CPU reset under breaking (see "2.17 Use Hook Function" for details). |