Configure the operating environment on the Property panel below when using E20.
Note that the contents of the Property panel differ depending on the communication method (FINE communications [E20(Serial)] or JTAG communications [E20(JTAG)]) between E20 and the target system.


Follow the steps below by selecting the corresponding tab on the Property panel.
2.3.3.1 [Connect Settings] tab
2.3.3.2 [Debug Tool Settings] tab