The files to download, as well as the download conditions applied at download time can be changed.
CS+ permits files in the following formats to be downloaded.
To change the download files, or set the download conditions applied at download time, use the Download Files dialog box shown below.
The Download Files dialog box is opened by clicking the [...] button that is displayed at the right edge in the column of the [Download files] property when you select it in the [Download] category on the Property panel's [Download File Settings] tab.


Here, a method on how to set in the Download Files dialog box shown above is described, using the following cases as examples.
2.5.2.1 Changing the download conditions for load module files
2.5.2.2 Adding a download file (*.hex, *.mot, or *.bin)
2.5.2.3 Downloading multiple load module files
2.5.2.4 Performing source-level debug with hex format, Motorola S format, or binary data format files
2.5.2.5 Downloading files to external flash memory [E1] [E20]