This panel displays operation logs for various components (design tool, build tool, etc.) provided by CS+.
The messages are classified by the message origination tool and displayed on the individual tabs.
The Message area can be zoomed in and out by |

The following items are explained here.
The output messages of each tool are displayed.
Note that the character colors/background colors of the message differ with the type of output message (and depend on the settings in the [General - Font and Color] category in the Option dialog box).
Select the tab that indicates the origin of message.
The following tabs are available for the Pin Configurator.
Displays operation logs for all components (design tool, build tool, etc.) provided by CS+ in order of output. |
Even if a new message is output on a deselected tab, tab selection will not automatically switch. In this case, " * " mark will be added in front of the tab name, indicating that a new message has been output. |
Sends the character string or lines selected with range selection to the clipboard. |
|
Selects all the messages displayed on the Message area. |
|
Deletes all the messages displayed on the Message area. |
|
Jumps to the caret line in the editor indicated by the message (file, line, and column). |
|
Displays help for the message on the current caret location. |