Everything

debugger.Interrupt.RequestEI


This function sends an EI-level interrupt request to the interrupt controller. [RH850 Simulator] [RH850G4MH, RH850G4KH]

[Specification format]

debugger.Interrupt.RequestEI(channel)

[Argument(s)]

Argument

Description

channel

Specify an interrupt name (string) or vector address (numeric value).

[Return value]

If the interrupt request was successful : True

If the interrupt request failed : False

[Detailed description]

-

This function sends an EI-level interrupt request to the interrupt controller.

-

Generation of the interrupt depends on the settings and state of the interrupt controller.

[Example of use]

>>>debugger.Interrupt.RequestEI(1)
True
>>>