Running and Stopping the Program
![]()

Now that download of the load module file to the target is complete, you can run the program. First, run and stop the program.
1. Running the program
Run the program after resetting CPU.
|
Click the [Restart] button in the menu. |


|
This runs the program and displays [RUN] in the status bar. |


|
LEDs on QB-R5F100LE-TB light alternately. |