This page displays a list of available updates. Select updates to download and install.

The following items are explained here.
From the CS+ Update Manager window menu area, click [All]. |
From the CS+ Update Manager window menu area, click [Microcontroller Name]. |
If a microcontroller was specified, the microcontroller name appears.
Displays a list of items to update.
Click [Select all] to select the check boxes of all updates.
The following information is displayed for each update.
This appears if there is detailed information about the update. Selecting it will display details in a browser. |
If an update is selected in the Update Selection area, it is completely hidden.