Use this category to configure general setting relating to update.

The following items are explained here.
Automatically checks for updates when a project is opened (default). |
|
Does not automatically check for updates when a project is opened. |
Specify the interval at which to check for updates.
Either enter a number between 0 and 99 directly via the keyboard, or specify a number via the
buttons.
Restores all settings on this dialog box to their default values. Note, however, that newly added items in the [General - External Tools] category will not be removed. |
|