1.4  Operating Environment
 
Below are the system requirements for this product.
Processor and main memory that can comfortably run the software described in the software environment
Display: Resolution at least 1,024 x 768
Interface: USB 2.0
-  | Microsoft .NET Framework 4.6.2  | 
 
-  | Microsoft Visual C++ 2015 Redistributable Update 3 (x86)  | 
 
-  | Microsoft Edge WebView2 Runtime  | 
 
-  | Online help: Edge, Chrome, or Firefox (The latest version is recommended)  | 
 
(3)  | Supported target environments  | 
 
-  | Full-spec emulator [RH850]  | 
 
-  | E2 emulator [RH850][RX][RL78]  | 
 
-  | E2 emulator Lite [RX][RL78]  |