Everything

Usage example

Start conversion digital input to analog signal from 0x00. Add 0x10 to digital input at fixed interval. Stop conversion when digital input becomes 0xFF.

 

[GUI setting example]

D/A convertor

Used

DAC

Used

DAC0

D/A convertor operation setting

Used

D/A convertor operation setting

Normal mode

Analog output (ANO0)

Used

Conversion value

0x00

 

Timer

Used

TAU0

Used

Channel0

channel 0

Interval timer

Interval value (16 bits)

100ms (Actual value:100)

Generates INTTM00 when counting is started

Unused

End of timer channel 0 count, generate an interrupt (INTTM00)

Used

Priority (INTTM00)

Low

 

 

[API setting example]

r_main.c

void main(void)

{

       R_MAIN_UserInit();

       /* Start user code. Do not edit comment generated here */

       /* Start TAU0 channel 0 counter */

       R_TAU0_Channel0_Start();

 

       /* Enable the DA converter channel 0 */

       R_DAC0_Start();

 

       while (1U)

       {

              ;

       }

       /* End user code. Do not edit comment generated here */

}

 

r_cg_timer_user.c

/* Start user code for include. Do not edit comment generated here */

#include "r_cg_dac.h"

/* End user code. Do not edit comment generated here */

 

/* Start user code for global. Do not edit comment generated here */

volatile uint16_t g_dac0_value = _00_DA0_CONVERSION_VALUE;

/* End user code. Do not edit comment generated here */

 

static void __near r_tau0_channel0_interrupt(void)

{

       /* Start user code. Do not edit comment generated here */

       g_dac0_value += 0x0010U;

       if (g_dac0_value <= 0x00FFU)

       {

              /* Set the DA converter channel 0 value */

              R_DAC0_Set_ConversionValue((uint8_t)g_dac0_value);

       }

       else

       {

              /* Stop the DA converter channel 0 */

              R_DAC0_Stop();

 

              /* Stop TAU0 channel 0 counter */

              R_TAU0_Channel0_Stop();

       }

       /* End user code. Do not edit comment generated here */

}