Everything

Usage example

Start data transfer by the end of A/D conversion.

(Get A/D conversion results of 4 pins and copy them to RAM. Then, calculate the average of the results.)

 

[GUI setting example]

DMA controller

Used

DMA0

Used

DMAoperation setting

Used

Transfer direction setting

SFR to internal RAM

Transfer data size setting

8 bits

SFR address

ADCR -  0x000fff1e

RAM address

0xffe00

Transfer byte count

4

Trigger signal

INTAD (Please set INTAD)

DMA0 transfer end interrupt (INTDMA0)

Used

Priority

Low

 

A/D convertor

Used

ADC

Used

A/D convertor operation setting

Used

Comparator operation setting

Operation

Resolution setting

8 bits

VREF(+) setting

VDD

VREF(-) setting

VSS

Trigger mode setting

Software trigger mode

Operation mode setting

Countinous select mode

ANI0 - ANI7 analog input selection

ANI0 - ANI3

A/D channel selection

ANI0 - ANI3

Conversion time mode

Normal 1

Conversion time

34 (1088/fCLK)(μs)

Conversion result upper/lower bound value setting

Generates an interrupt request (INTAD) when ADLL≦ADCRH≦ADUL

Upper bound (ADUL) value

255

Lower bound (ADLL) value

0

Use  A/D interrupt (INTAD)

Used

 

 

[API setting example]

r_main.c

void main(void)

{

       R_MAIN_UserInit();

       /* Start user code. Do not edit comment generated here */

       /* Enable DMA0 transfer */

       R_DMAC0_Start();

 

       /* Start the AD converter */

       R_ADC_Start();

 

       while (1U)

       {

              NOP();

       }

       /* End user code. Do not edit comment generated here */

}

 

 

 

r_cg_dmac_user.c

/* Start user code for include. Do not edit comment generated here */

#include "r_cg_adc.h"

/* End user code. Do not edit comment generated here */

 

/* Start user code for pragma. Do not edit comment generated here */

#pragma address (g_adc_buf = 0x0ffe00)

/* End user code. Do not edit comment generated here */

 

/* Start user code for global. Do not edit comment generated here */

volatile uint8_t g_adc_buf[5][4];

volatile uint8_t g_adc_buf_cnt = 0U;

/* End user code. Do not edit comment generated here */

 

static void __near r_dmac0_interrupt(void)

{

       /* Start user code. Do not edit comment generated here */

       uint8_t i;

       uint8_t j;

       uint16_t temp;

 

       /* Stop the AD converter */

       R_ADC_Stop();

 

       /* Disable DMA0 transfer */

       R_DMAC0_Stop();

 

       /* Change DMA0_RAM address */

       if ((++g_adc_buf_cnt) < 4U)

       {

              DRA0 += 4U;

       }

       else

       {

              DRA0 = _FE00_DMA0_RAM_ADDRESS;

              g_adc_buf_cnt = 0U;

 

              /* Calculate the average */

              for (i = 0; i < 4U; i++)

              {

                     temp = 0U;

                     for (j = 0; j < 4U; j++)

                     {

                            temp += g_adc_buf[j][i];

                     }

                     g_adc_buf[4][i] = temp / 4U;

              }

       }

 

       /* Enable DMA0 transfer */

       R_DMAC0_Start();

 

       /* Start the AD converter */

       R_ADC_Start();

       /* End user code. Do not edit comment generated here */

}