Everything

Usage example

Reset by Oscillation stop detection interrup.

 

[GUI setting example]

Oscillation stop detector

Used

OSCSTOPDETECTOR

Used

Oscillation stop detector operation setting

Used

Oscillation stop judgement time

100(ms) (TYP.) (Actual value:100)

Generate an interrupt when oscillation stop is detected (INTOSDC)

Used

Priority

Low

 

Watchdog timer

WDT

Used

Watchdog timer operationsetting

Used

Operation in HALT/STOP/SNOOZE mode setting

Enaled

Overflow time

2^16/fIL 4369.07(ms)

Window open period

100(%)

Enable interval interruptwhen 75% + 1/2fIL of overflow time (INTWDTI)

Used

Priority

Low

 

 

 

[API setting example]

r_main.c

void main(void)

{

       R_MAIN_UserInit();

       /* Start user code. Do not edit comment generated here */

       /* Start OSDC module operation */

       R_OSDC_Start();

 

       while (1U)

       {

              /* Restart the watchdog timer */

              R_WDT_Restart();

       }

       /* End user code. Do not edit comment generated here */

}

 

r_cg_osdc_user.c

static void __near r_osdc_interrupt(void)

{

       /* Start user code. Do not edit comment generated here */

       /* Stop OSDC module operation */

       R_OSDC_Stop();

 

       /* End user code. Do not edit comment generated here */

}