|
Section address operator (__sectop/__secend)
|
This is a section address operator.
[Function]
- | __sectop returns the start address of the specified section-name. |
- | __secend returns the end address of the specified section-name +1. |
- | The return type of __sectop( ) and __secend( ) is void __far*. |
- | Addition and subtraction between the value obtained by __sectop or __secend and a constant should not be used. |
[Usage]
__sectop("section-name")
__secend("section-name")
|
[Example]
The following shows a sample C source code.
const struct {
void __far *rom_s;
void __far *rom_e;
} DTBL[]={__sectop("XXX"), __secend("XXX")};
|
The following shows the declarations in the assembly source code.
.PUBLIC _DTBL
.SECTION .const, CONST
.ALIGN 2
_DTBL:
.DB2 LOWW(STARTOF(XXX)) ;Lower-order 2 bytes of rom_s
.DB LOW(HIGHW(STARTOF(XXX))) ;Least significant byte rom_s
.DB 0x00
.DB2 LOWW(STARTOF(XXX)+SIZEOF(XXX)) ;Lower-order 2 bytes of rom_e
.DB LOW(HIGHW(STARTOF(XXX)+SIZEOF(XXX))) ;Least significant byte rom_e
.DB 0x00
|