|
|
|
|
__DI
|
Outputs a DI instruction.
|
void __DI(void);
|
__EI
|
Outputs a EI instruction.
|
void __EI(void);
|
__halt
|
Outputs a HALT instruction.
|
void __halt(void);
|
__stop
|
Outputs a STOP instruction.
|
void __stop(void);
|
__brk
|
Outputs a BRK instruction.
|
void __brk(void);
|
__nop
|
Outputs a NOP instruction.
|
void __nop(void);
|
__rolb
|
Rotates x to the left y times assuming that x has a size of eight bits.
Operation is undefined for the case where the rotation count is greater than the size of the value.
If the rotation count may be greater than the size, mask the count to not exceed the size.
|
unsigned char __rolb(
unsigned char x,
unsigned char y
);
|
__rorb
|
Rotates x to the right y times assuming that x has a size of eight bits.
Operation is undefined for the case where the rotation count is greater than the size of the value.
If the rotation count may be greater than the size, mask the count to not exceed the size.
|
unsigned char __rorb(
unsigned char x,
unsigned char y
);
|
__rolw
|
Rotates x to the left y times assuming that x has a size of 16 bits.
Operation is undefined for the case where the rotation count is greater than the size of the value.
If the rotation count may be greater than the size, mask the count to not exceed the size.
|
unsigned int __rolw(
unsigned int x,
unsigned char y
);
|
__rorw
|
Rotates x to the right y times assuming that x has a size of 16 bits.
Operation is undefined for the case where the rotation count is greater than the size of the value.
If the rotation count may be greater than the size, mask the count to not exceed the size.
|
unsigned int __rorw(
unsigned int x,
unsigned char y
);
|
__mulu
|
Executes unsigned multiplication between (unsigned int)x and (unsigned int)y and returns a 16-bit result.
|
unsigned int __mulu(
unsigned char x,
unsigned char y
);
|
__mului
|
Executes unsigned multiplication between (unsigned long)x and (unsigned long)y and returns a 32-bit result.
|
unsigned long __mului(
unsigned int x,
unsigned int y
);
|
__mulsi
|
Executes signed multiplication between (signed long)x and (signed long)y and returns a 32-bit result.
|
signed long __mulsi(
signed int x,
signed int y
);
|
__mulul
|
Executes unsigned multiplication between (unsigned long long)x and (unsigned long long)y and returns a 64-bit result. When the -lang=c and -strict_std options are specified, this function is not defined as an intrinsic function.
|
unsigned long long __mulul(
unsigned long x,
unsigned long y
);
|
__mulsl
|
Executes signed multiplication between (signed long long)x and (signed long long)y and returns a 64-bit result. When the -lang=c and -strict_std options are specified, this function is not defined as an intrinsic function.
|
signed long long __mulsl(
signed long x,
signed long y
);
|
__divui
|
Executes unsigned division between x and y and returns a 16-bit result.
When divisor y is 0, 0xFFFF is returned.
|
unsigned int __divui(
unsigned int x,
unsigned char y
);
|
__divul
|
Executes unsigned division between x and y and returns a 32-bit result.
When divisor y is 0, 0xFFFFFFFF is returned.
|
unsigned long __divul(
unsigned long x,
unsigned int y
);
|
__remui
|
Executes unsigned remainder operation between x and y and returns a 8-bit result.
When divisor y is 0, the lower-order 8 bits of dividend x are returned.
|
unsigned char __remui(
unsigned int x,
unsigned char y
);
|
__remul
|
Executes unsigned remainder operation between x and y and returns a 16-bit result.
When divisor y is 0, the lower-order 16 bits of dividend x are returned.
|
unsigned int __remul(
unsigned long x,
unsigned int y
);
|
__macui
|
Executes unsigned multiply-accumulate operation (unsigned long) x * (unsigned long) y + z, and returns a 32-bit result.
|
unsigned long __macui(
unsigned int x,
unsigned int y,
unsigned long z
);
|
__macsi
|
Executes unsigned multiply-accumulate operation (signed long) x * (signed long) y + z, and returns a 32-bit result.
|
signed long __macsi(
signed int x,
signed int y,
signed long z
);
|
__get_psw
|
Returns the contents of PSW.
|
unsigned char __get_psw(void);
|
__set_psw
|
Sets x to PSW.
|
void __set_psw(unsigned char x);
|
__set1
|
The set1 instruction is used to set bit y of the address indicated by x to 1.
Only a constant from 0 to 7 can be specified for bit y and a compile error will occur when any other value is specified.
|
void __set1(
unsigned char __near *x,
unsigned char y
);
|
__clr1
|
The clr1 instruction is used to clear bit y of the address indicated by x to 0.
Only a constant from 0 to 7 can be specified for bit y and a compile error will occur when any other value is specified.
|
void __clr1(
unsigned char __near *x,
unsigned char y
);
|
__not1
|
The not1 instruction (xor instruction for the saddr area) is used to invert bit y of the address indicated by x.
Only a constant from 0 to 7 can be specified for bit y and a compile error will occur when any other value is specified.
|
void __not1(
unsigned char __near *x,
unsigned char y
);
|
__delay_cycles
|
Waits for the number of cycles specified with the cycles argument. Only a constant from 1 to 83886097 can be specified for cycles. If any other value is specified, a compile error occurs.
The actual number of cycles to wait might be greater than the specified value.
|
void __delay_cycles(unsigned long cycles);
|