You can launch CS+ from the command line (e.g. the Windows command prompt), and control it via command input without displaying the Main window.
This section describes the control of CS+ when launched from the Windows command prompt.
From the command prompt, execute CubeSuite+.exe or CubeSuiteW+.exe, located in the CS+ installation folder.
If you execute CubeSuite+.exe, you can launch CS+, load plug-ins, and execute builds without displaying the Main window.
The format to specify on the command line is shown below.
{}|: When options are separated by pipeline characters ("|"), any one of the options can be specified
...: Pattern in proceeding [ ] can be repeated
Each option is described below.
|
Launch CS+ without displaying the Main window, and exit without performing any actions. |
||||
/bbΔ[build-mode-name] |
Launch without displaying the Main window, build all the projects included in specified project-file-name, with the build mode specified by build-mode-name, and then exit. If a project does not have the build mode specified by build-mode-name, then the build mode is copied based on the DefaultBuild, and the build is performed. If the build mode specified by build-mode-name is not defined in the project specified by project-file-name, then an error will be displayed, and processing will end. If build-mode-name is omitted, then the build will use the DefaultBuild. If project-file-name is omitted, then an error will be displayed, and processing will end. |
|||
/brΔ[build-mode-name] |
Launch without displaying the Main window, build all the projects included in specified project-file-name, with the build mode specified by build-mode-name, and then exit. If a project does not have the build mode specified by build-mode-name, then the build mode is copied based on the DefaultBuild, and the build is performed. If the build mode specified by build-mode-name is not defined in the project specified by project-file-name, then an error will be displayed, and processing will end. If build-mode-name is omitted, then the build will use the DefaultBuild. If project-file-name is omitted, then an error will be displayed, and processing will end. |
|||
/bcbΔ[build-mode-name] |
Perform a clean and then execute a build. Launch without displaying the Main window, build all the projects included in specified project-file-name, with the build mode specified by build-mode-name, and then exit. If a project does not have the build mode specified by build-mode-name, then the build mode is copied based on the DefaultBuild, and the build is performed. If the build mode specified by build-mode-name is not defined in the project specified by project-file-name, then an error will be displayed, and processing will end. If build-mode-name is omitted, then the build will use the DefaultBuild. If project-file-name is omitted, then an error will be displayed, and processing will end. |
|||
/bcΔ[build-mode-name] |
Launch without displaying the Main window, build all the projects included in specified project-file-name, with the build mode specified by build-mode-name, and then exit. If a project does not have the build mode specified by build-mode-name, then the build mode is copied based on the DefaultBuild, and the build is performed. If the build mode specified by build-mode-name is not defined in the project specified by project-file-name, then an error will be displayed, and processing will end. If build-mode-name is omitted, then the build will use the DefaultBuild. If project-file-name is omitted, then an error will be displayed, and processing will end. |
|||
/bol |
Execute [Build Option List]. Options for all build modes are displayed, in the same way as when executing [Build] - [Build Options List]. If a project-file-name is omitted, then an error will be displayed, and processing will end. |
|||
/odpΔ[of=output-folder-path][Δbuild-mode-name] |
Output a dependency-information file. This option outputs a dependency-information file, and then exit the program without displaying the Main window. The file to be output includes the dependency information in the build mode specified with build-mode-name of all projects in the project file specified with project-file-name. When of=output-folder-path is specified, the file is output to the specified folder (the folder is created if not already present). When of=output-folder-path is omitted, a subfolder with a name of the form "QualityRecordYYYYMMDDThhmmss" is automatically created in the project folder for output of the file. If build-mode-name is omitted, DefaultBuild is used as the build mode for the output of the file. If project-file-name is omitted, an error message will be displayed and processing will abort. The output format is the same as that for dependency information that is output with [Output Data for Quality Records Collectively] in the Smart Report dialog box. The name of the output file is <project name>.deps. |
|||
/cve |
Convert a project for CA78K0R or CA78K0 to one for CC-RL and output a common project file (*.rcpe).
Launch without opening the Main window, convert all the projects included in specified project-file-name, and then exit. The output folder is the same folder as that of project-file-name, and the output file name is the same as project-file-name with its extension changed to ".rcpe". The device of the project and subprojects of the conversion source is directly used as the device of conversion destination. If project-file-name is omitted, then an error will be displayed, and processing will end. |
|||
/lpΔplug-in-name[,plug-in-name,...] |
Start CS+ without displaying the Main window, and with loading the specified plug-ins in the Plugins folder. In plug-in-name, specify the name of the folder in which each DLL file is saved. However, if the name of the folder is “plugin name_nnn” (nnn is a decimal value), the file name does not include “_nnn”.Note that folder names are case-insensitive. You can specify multiple plug-in names by separating them with commas. You can also specify the "/lp" option itself multiple times. Each DLL will be loaded. When a plug-in with the same name is specified for the /np option, the option specified backward of the command line will take precedence. If the plug-in specified by this option does not exist, it will be ignored. If project-file-name is omitted, then an error will be displayed, and processing will end. |
|||
/lpall |
Start CS+ without displaying the Main window, and with loading all plugins in the Plugins folder. If this is specified together with the "/np" or “/lp” option, then this option will take precedence. When a plug-in is specified together with the /npall option, the option specified backward of the command line will take precedence. If project-file-name is omitted, then an error will be displayed, and processing will end. |
|||
/npΔplug-in-name[,plug-in-name,...] |
Start CS+ without displaying the Main window, and without loading the specified plugins in the Plugins folder. In plug-in-name, specify the name of the folder in which each DLL file is saved. However, if the name of the folder is “plugin name_nnn” (nnn is a decimal value), the file name does not include “_nnn”.Note that folder names are case-insensitive. You can specify multiple plug-in names by separating them with commas. You can also specify the "/np" option itself multiple times. Each DLL will not be loaded. When a plug-in with the same name is specified for the /lp option, the option specified backward of the command line will take precedence. If the plug-in specified by this option does not exist, it will be ignored. If project-file-name is omitted, then an error will be displayed, and processing will end. |
|||
/npall |
Start CS+ without displaying the Main window, and without loading any of the specified plugins in the Plugins folder. If this is specified together with the "/np" or “/lp” option, then this option will take precedence. When a plug-in is specified together with the /lpall option, the option specified backward of the command line will take precedence. If project-file-name is omitted, then an error will be displayed, and processing will end. |
|||
/langΔlanguage-for-display |
Specify this option when the language for display is different from that for the OS.Note |
|||
plug-in-optionΔ[plug-in-parameter,...] |
Specify an option for the plug-in (see "(3) Plug-in Options"). |
|||
project-file-name |
Start CS+ without displaying the Main window, with the specified project file (with ".mtpj" extension) loaded. |
|||
When the "/lp", "/lpall", "/np", or "/npall" option is specified, the settings of the Plug-in Manager dialog box are not changed. |
When the /bb, /br, or /bcb option is specified, the build is run in accord with the setting of the [General - Build] category in the Option dialog box. For example, when [Project folder] is selected for [Output destination of the result of updating dependencies], a dependency-information file is output to the project folder. |
Names such as event names that have been saved in the project file (*.mtpj or *.mtud) or Information set for each user of the PC (c1_user.mtpu) will be displayed as they are. |
If "ja-JP" is specified for /lang in a non-Japanese OS, text in the messages output by the CC-RL and CC-RH compilers will be garbled. |
The results of execution are output to the command prompt.
Execute CubeSuiteW+.exe to launch CS+, displaying the Main window and with plugins loaded, in the same manner as when launching it from the [Start] menu.
The format to specify on the command line is shown below.
...: Pattern in proceeding [ ] can be repeated
Each option is described below.
|
Start CS+ with the Main window displayed, in the same manner as when launching it from the [Start] menu. |
||
/lpΔplug-in-name[,plug-in-name,...] |
Start CS+ displaying the Main window, with loading the specified plugins in the Plugins folder. In plug-in-name, specify the name of the folder in which the DLL file is saved. However, if the name of the folder is “plugin name_nnn” (nnn is a decimal value), the file name does not include “_nnn”. Note that folder names are case-insensitive. You can specify multiple plug-in names by separating them with commas. You can also specify the "/lp" option itself multiple times. Each DLL will be loaded. When a plug-in with the same name is specified for the /np option, the option specified backward of the command line will take precedence. If the plug-in specified by this option does not exist, it will be ignored. |
|
/lpall |
Start CS+ displaying the Main window, with loading all plug-ins in the Plugins folder. |
|
/npΔplug-in-name[,plug-in-name,...] |
Start CS+ displaying the Main window, without loading the specified plugins in the Plugins folder. In plug-in-name, specify the name of the folder in which the DLL file is saved. However, if the name of the folder is “plugin name_nnn” (nnn is a decimal value), the file name does not include “_nnn”.Note that folder names are case-insensitive. You can specify multiple plug-in names by separating them with commas. You can also specify the "/np" option itself multiple times. Each DLL will not be loaded. When a plug-in with the same name is specified for the /lp option, the option specified backward of the command line will take precedence. If the plug-in specified by this option does not exist, it will be ignored. |
|
/npall |
Start CS+ displaying the Main window, without loading any of the specified plug-ins in the Plugins folder. |
|
/noproj |
Start CS+ displaying the Main window without reading in a project (either a project specified on the command line, or the last used project). |
|
/nrs |
If CS+ is already started and in the standby state using rapid start (see "2.2 Start CS+"), ignore this and start another process. |
|
/langΔlanguage-for-display |
Specify this option when the language for display is different from that for the OS.Note 1 |
|
plug-in-optionΔ[plug-in-parameter,...] |
Specify an option for the plug-in (see "(3) Plug-in Options"). |
|
project-file-name |
Start CS+ displaying the Main window, with the specified project file (with ".mtpj" extension) loaded. |
|
When the "/lp", "/lpall", "/np", or "/npall" option is specified, the settings of the Plug-in Manager dialog box are not changed. |
Names such as event names that have been saved in the project file (*.mtpj or *.mtud) or Information set for each user of the PC (c1_user.mtpu) will be displayed as they are. |
The display of the [Cancel] button in the Confirm Toolbar Reset dialog box, which is displayed by clicking on the [Reset…] button on the [Toolbars] tab in the User Setting dialog box, will be written in Japanese. |
Below are the plug-in options that can be specified.