Everything

 

-Xcpu


This option specifies that an object for the specified core is generated.

[Specification format]

-Xcpu=core

 

-

Interpretation when omitted

An object for G3M is generated.

[Detailed description]

-

This option specifies that an object for core core is generated.

-

The items that can be specified as core are shown below.

g3m

Generates an object for G3M.

g3k

Generates an object for G3K.

g3mh

Generates an object for G3MH. [V1.02.00 or later]

g3kh

Generates an object for G3KH. [V1.03.00 or later]

g4mh

Generates an object for G4MH. [V2.00.00 or later]

g4kh

Generates an object for G4KH. [V2.05.00 or later]

 

-

If this option is specified more than once, the last specification is valid.

-

An error will occur in any of the following cases.

-

When the parameter is omitted

-

When a parameter that is not specifiable is specified