Control instructions provide detailed instructions for assembler operation and so are written in the source.
Control instructions do not become the target of object code generation.
Control instruction categories are displayed below.
As with directives, control instructions are specified in the source.
Control instructions must be specified at the beginning of a line in the same way as for preprocessing directives in C language.