< Compile Options / Microcontroller Options >
This option is used to perform compilation conforming to the specifications specific to the CPU type. |
When -patch=rx610 is specified, any MVTIPL instructions not supported by the RX610 Group are not used in the generated code. A value from 0 to 7 can be specified for the argument of the intrinsic function set_ipl. |