Everything

-MMD [V3.08.00 or later]


< Assembler Command Options / Dependency File Output Specification Options >

[Format]

-MMD

 

-

[Default]

No dependency file is output.

[Description]

-

This option outputs the dependencies of the input file, as specified by the .INCLUDE assembler directive, to the dependency file in makefile format. It also executes assembling.

-

The output file name is the same as the input file name, with the extension replaced by “dep”.

[Remarks]

-

When multiple input files are specified, only the dependency file for the last input file is output.