Everything
3.2.2 Option Information

The option strings specified by a command line or a subcommand file are output. The following figure shows an example of option information output when rlink -subcommand=test.sub -list -show is specified.

(test.sub contents)
INPUT test .obj
*** Options ***
-subcommand=test.sub (1)
INPUT test .obj      (2)
-list                (1)
-show                (1)

Item Number

Description

(1)

Outputs option strings specified by a command line or a subcommand in the specified order.

(2)

Subcommand in the test.sub subcommand file.