Everything
4.1.4 Implementation-defined behavior of C99

(1)

How a diagnostic is identified (3.10, 5.1.1.3).

Refer to "10. MESSAGES".

(2)

Whether each non-empty sequence of white-space characters other than new-line is retained or replaced by one space character in translation phase 3 (5.1.1.2).

Retained as they are.

(3)

The mapping between physical source file multi-byte characters and the source character set in translation phase 1 (5.1.1.2).

Multibyte characters are mapped to the corresponding source character set according to the compile option.

(4)

The name and type of the function called at program startup in a freestanding environment (5.1.2.1).

Not defined. Depends on the startup implementation.

(5)

The effect of program termination in a freestanding environment (5.1.2.1).

Depends on startup in a normal termination. Create an exit processing routine if the program needs to terminate abnormally.

(6)

An alternative manner in which the main function may be defined (5.1.2.2.1).

Not defined because of a freestanding environment.

(7)

The values given to the strings pointed to by the argv argument to main (5.1.2.2.1).

Not defined because of a freestanding environment.

(8)

What constitutes an interactive device (5.1.2.3).

Not defined for the configuration of an interactive device.

(9)

The set of signals, their semantics, and their default handling (7.14).

The signal handling functions are not supported.

(10)

Signal values other than SIGFPE, SIGILL, and SIGSEGV that correspond to a computational exception (7.14.1.1).

The signal handling functions are not supported.

(11)

Signals for which the equivalent of signal(sig, SIG_IGN); is executed at program startup (7.14.1.1).

The signal handling functions are not supported.

(12)

The set of environment names and the method for altering the environment list used by the getenv function (7.20.4.5).

The getenv function is not supported.

(13)

The manner of execution of the string by the system function (7.20.4.6).

The system function is not supported.

(14)

Which additional multibyte characters may appear in identifiers and their correspondence to universal character names (6.4.2).

Multibyte characters cannot be used as identifiers.

(15)

The number of significant initial characters in an identifier (5.2.4.1, 6.4.2).

The entire identifier is handled as meaningful. The length of an identifier is unlimited.

(16)

The number of bits in a byte (3.6).

8 bits.

(17)

The values of the members of the execution character set (5.2.1).

The element values of the execution character set are ASCII code, EUC, SJIS, UTF-8, big5 and gb2312 values.

(18)

The unique value of the member of the execution character set produced for each of the standard alphabetic escape sequences (5.2.2).

Escape Sequence

Value (ASCII)

"\a"

0x07

"\b"

0x08

"\f"

0x0C

"\n"

0x0A

"\r"

0x0D

"\t"

0x09

"\v"

0x0B

(19)

The value of a char object into which has been stored any character other than a member of the basic execution character set (6.2.5).

Value that is type-converted to char type.

(20)

Which of signed char or unsigned char has the same range, representation, and behavior as "plain" char (6.2.5, 6.3.1.1).

The char type has the same range of values, the same representation format and the same behavior as the unsigned char type. However, it can be switched to the signed char type by the -signed_char option.

(21)

The mapping of members of the source character set (in character constants and string literals) to members of the execution character set (6.4.4.4, 5.1.1.2).

When the character code selection of the input program is the same as the character code selection of the output file according to an option specification, association with the element having the same value is performed. If they are different according to the option specification, the value of the corresponding character code is used.

(22)

The value of an integer character constant containing more than one character or containing a character or escape sequence that does not map to a single-byte execution character (6.4.4.4).

A integer character constant consisting of up to four characters has a four-byte value with the lower byte being the last character and the upper byte being the first character. A character constant having five or more characters results in an error. A character which is not represented by basic execution environment character set is regarded as a integer character constant having that value. In an invalid escape sequence, the backslash is ignored and the next character is regarded as a integer character constant.

(23)

The value of a wide character constant containing more than one multibyte character, or containing a multibyte character or escape sequence not represented in the extended execution character set (6.4.4.4).

Left-most character value as a multibyte character.

(24)

The current locale used to convert a wide character constant consisting of a single multi-byte character that maps to a member of the extended execution character set into a corresponding wide character code (6.4.4.4).

Locale is not supported.

(25)

The current locale used to convert a wide string literal into corresponding wide character codes (6.4.5).

Locale is not supported.

(26)

The value of a string literal containing a multi-byte character or escape sequence not represented in the execution character set (6.4.5).

Corresponding byte value for escape sequence or corresponding each byte value for a multibyte character.

(27)

Any extended integer types that exist in the implementation (6.2.5).

No extended integer types are provided.

(28)

Whether signed integer types are represented using sign and magnitude, two's complement, or one's complement, and whether the extraordinary value is a trap representation or an ordinary value (6.2.6.2).

The signed integer type is represented in two's complement, and there are no trap representations.

(29)

The rank of any extended integer type relative to another extended integer type with the same precision (6.3.1.1).

No extended integer types are provided.

(30)

The result of, or the signal raised by, converting an integer to a signed integer type when the value cannot be represented in an object of that type (6.3.1.3).

Bit string masked by the width of the conversion target type (with the upper bits truncated).

(31)

The results of some bit-wise operations on signed integers (6.5).

Arithmetic shift is performed for a shift operator. For other operators, a signed integer is calculated as an unsigned value (as a bit image).

(32)

The accuracy of the floating-point operations and of the library functions in <math.h> and <complex.h> that return floating-point results (5.2.4.2.2).

Unknown.

(33)

The rounding behaviors characterized by non-standard values of FLT_ROUNDS (5.2.4.2.2).

No nonstandard value is defined for FLT_ROUNDS.

(34)

The evaluation methods characterized by non-standard negative values of FLT_EVAL_METHOD (5.2.4.2.2).

No nonstandard value is defined for FLT_EVAL_METHOD.

(35)

The direction of rounding when an integer is converted to a floating-point number that cannot exactly represent the original value (6.3.1.4).

Rounded to the nearest direction if any of these conditions is met:

-nofpu is specified.

-cpu=rx200 is specified.

-cpu=rx600 or -isa=rxv1 is specified and the integer to be converted is unsigned.

Otherwise, the setting in the RM[0:1] bits in FPSW is followed.

[V3.01.00 or later] When -dpfpu is specified, the result of conversion to the double-precision floating-point type is in accord with the setting of the DRM[0:1] bits in the DPSW.

(36)

The direction of rounding when a floating-point number is converted to a narrower floating-point number (6.3.1.5).

As per the option (-round) specification and microcomputer settings.

(37)

How the nearest representable value or the larger or smaller representable value immediately adjacent to the nearest representable value is chosen for certain floating constants (6.4.4.2).

As per the option (-round) specification.

(38)

Whether and how floating expressions are contracted when not disallowed by the FP_CONTRACT pragma (6.5).

Contraction of expressions depends on each option specification.

The FP_CONTRACT pragma does not work.

#pragma STDC FP_CONTRACT is ignored even if it is specified.

(39)

The default state for the FENV_ACCESS pragma (7.6.1).

The default state of the FENV_ACCESS pragma is ON.

#pragma STDC FENV_ACCESS is ignored even if it is specified.

(40)

Additional floating-point exceptions, rounding modes, environments, and classifications, and their macro names (7.6, 7.12).

As per the math.h and fenv.h libraries provided by the compiler. There are no additional definitions.

(41)

The default state for the FP_CONTRACT pragma (7.12.2).

The default state of the FP_CONTRACT pragma is ON.

(42)

Whether the "inexact" floating-point exception can be raised when the rounded result actually does equal the mathematical result in an IEC 60559 conformant implementation (F.9).

No "inexact" floating-point exception is generated for the nearbyint, nearbyintf or nearbyintl function. An "inexact" floating-point exception may be generated for the rint, rintf or rintl function.

(43)

Whether the underflow (and inexact) floating-point exception can be raised when a result is tiny but not inexact in an IEC 60559 conformant implementation (F.9).

As per the option (-round) specification and microcomputer settings.

(44)

The result of converting a pointer to an integer or vice versa (6.3.2.3).

-

Integer-to-pointer conversion result
If the size of an integer type is larger than that of a pointer type, the lower-byte value of the integer type is used. If the size of the integer type is equal to that of the pointer type, the bit pattern of the integer type is retained as is. If the size of the integer type is smaller than that of the pointer type, the resultant value of an extension to a long type is retained as is.

-

Pointer-to-integer conversion result
If the size of a pointer type is larger than that of an integer type, the lower-byte value of the pointer type is used. If the size of the pointer type is equal to that of the integer type, the bit pattern of the pointer type is retained as is. If the size of a pointer type is smaller than that of an integer type, the zero-extended value of the pointer type is used.

(45)

The size of the result of subtracting two pointers to elements of the same array (6.5.6).

The resultant type is the signed long type.

(46)

The extent to which suggestions made by using the register storage-class specifier are effective (6.7.1).

User requests for register variables are not honored.

(47)

The extent to which suggestions made by using the inline function specifier are effective (6.7.4).

Expansion is attempted only when the -inline option is valid. In addition, expansion may not be performed depending on the condition.

(48)

Whether a "plain" int bit-field is treated as signed int bit-field or as an unsigned int bit-field (6.7.2, 6.7.2.1).

Treated as an unsigned int type. However, this can be changed by the -signed_bitfield option.

(49)

Allowable bit-field types other than _Bool, signed int, and unsigned int (6.7.2.1).

All integer types are allowed.

(50)

Whether a bit-field can straddle a storage-unit boundary (6.7.2.1).

When structure type packing is not specified, a bit-field cannot straddle a strage-unit boundary, but it is allocated to the next area.

When structure type packing is specified, a bit-field may straddle a strage-unit boundary.

(51)

The order of allocation of bit-fields within a unit (6.7.2.1).

Allocated from the lower order. Selectable by the -bit_order option or #pragma bit_order.

(52)

The alignment of non-bit-field members of structures (6.7.2.1).

Refer to "4.1.5 Internal Data Representation and Areas".

(53)

The integer type compatible with each enumerated type (6.7.2.2).

Signed long type. However, the minimum type that an enumerated type fits in if the -auto_enum option is specified.

(54)

What constitutes an access to an object that has volatile-qualified type (6.7.3).

Although the order and number of accesses are as described in the C source, this does not apply to those accesses to a type for which the microcomputer does not have a corresponding instruction. An object qualified as volatile might be accessed in a smaller size than a declaration type.

(55)

How sequences in both forms of header names are mapped to headers or external source file names (6.4.7).

A character string described in the #include is interpreted as the character code specified as the source character set and is associated with a header name or an external source file name.

(56)

Whether the value of a character constant in a constant expression that controls conditional inclusion matches the value of the same character constant in the execution character set (6.10.1).

A value for the character constant specified in conditional inclusion is equal to the character constant value that appears in other expressions.

(57)

Whether the value of a single-character character constant in a constant expression that controls conditional inclusion may have a negative value (6.10.1).

(58)

The places that are searched for an included < > delimited header, and how the places are specified other header is identified (6.10.2).

Folders are searched in this order and a file having the same name in the folder is identified as the header.

1. Folder specified by the path (if it is full-path)

2. Folder specified by the -include option

3. Standard include file folder specified in the INC_RXA environment variable

(59)

How the named source file is searched for in an included " " delimited header (6.10.2).

Searched in this order:

1. Folder specified by the path (if it is full-path)

2. Folder having the source file

3. Folder specified by the -include option

4. Standard include file folder specified in the INC_RXA environment variable

(60)

The method by which preprocessing tokens (possibly resulting from macro expansion) in a #include directive are combined into a header name (6.10.2).

Treated as a preprocessing token of a single header or file name only in a macro that replaces preprocessing tokens with a single <character string> or "character string" format.

(61)

The nesting limit for #include processing (6.10.2).

There are no limits.

(62)

Whether the # operator inserts a \ character before the \ character that begins a universal character name in a character constant or string literal (6.10.3.2).

A \ character is not inserted in front of the first \ character.

(63)

The behavior on each recognized non-STDC #pragma directive (6.10.6).

Refer to "4.2.3 #pragma Directive".

(64)

The definitions for __DATE__ and __TIME__ when respectively, the date and time of translation are not available (6.10.8).

A date and time are always obtained.

(65)

Any library facilities available to a freestanding program, other than the minimal set required by clause 4 (5.1.2.1).

Refer to "7. LIBRARY FUNCTIONAL SPECIFICATION".

(66)

The format of the diagnostic printed by the assert macro (7.2.1.1).

As follows:

Assertion failed: Expression FILE file-name,LINE line-number FUNCNAME function-name

(67)

The representation of the floating-point status flags stored by the fegetexceptflag function (7.6.2.2).

One or combination of the following:

_FE_DIVBYZERO 0x04

_FE_INEXACT 0x10

_FE_INVALID 0x01

_FE_OVERFLOW 0x02

_FE_UNDERFLOW 0x08

(68)

Whether the feraiseexcept function raises the "inexact" floating-point exception in addition to the "overflow" or "underflow" floating-point exception (7.6.2.3).

An "inexact" floating-point exception may be generated if the E0 flag is set to 0 when an "overflow" floating-point exception is generated. Otherwise, no "inexact" floating-point exception is generated.

(69)

Strings other than "C" and "" that may be passed as the second argument to the setlocale function (7.11.1.1).

The setlocale function is not supported.

(70)

The types defined for float_t and double_t when the value of the FLT_EVAL_METHOD macro is less than zero or greater than two (7.12).

float_t is defined as the float type and double_t as the double type.

(71)

Domain errors for the mathematics functions, other that those required by this International Standard (7.12.1).

Refer to (72).

(72)

The values returned by the mathematics functions on domain errors (7.12.1).

acosh function group

The argument is x. If x < 1 is true, a domain error occurs. In this case, the return value is a NaN.

atanh function group

The argument is x. If -1 < x < 1 is true, a domain error occurs. In this case, the return value is a NaN.

ccosh function group

The argument is x.

- If the real part of x is 0 and the imaginary part of x is ±∞, a domain error occurs. In this case, the return value is NaN + 0 × i.

- If the real part of x is ±∞ and the imaginary part of x is ±∞, a domain error occurs. In this case, the return value is ∞ + NaN × i.

- If the real part of x is a finite value and the imaginary part of x is ±∞, a domain error occurs. In this case, the return value is NaN + NaN × i.

cexp function group

The argument is x.

- If the real part of x is +∞ and the imaginary part of x is ±∞, a domain error occurs. In this case, the return value is +∞ + NaN × i.

- If the real part of x is a finite value and the imaginary part of x is ±∞, a domain error occurs. In this case, the return value is NaN + NaN × i

csinh function group

The argument is x.

- If the real part of x is 0 or ±∞ and the imaginary part of x is ±∞, a domain error occurs. In this case, the return value is the real part of x + NaN × i.

- If the real part of x is a finite value and the imaginary part of x is ±∞, a domain error occurs. In this case, the return value is NaN + NaN × i.

fma function group

The first argument is x1, the second argument is x2, and the third argument is x3.

- If x1 is ±∞, x2 is 0, and x3 is not a NaN, a domain error occurs. In this case, the return value is a NaN.

- If x1 is 0 , x2 is ±∞, and x3 is not a NaN, a domain error occurs (no definition). In this case, the return value is a NaN.

- If x1, x2, and x3 are ±∞ and the sign of x1 and x2 is different from that of x3, (that is, subtraction between ∞ occurs), a domain error occurs. In this case, the return value is a NaN.

llrint function group

The argument is x.

- If x is a finite value that cannot be represented in the longlong type, a domain error occurs. In this case, the return value is 0.

- If x is a NaN or ±∞, a domain error occurs. In this case, the return value is 0.

llround function group

The argument is x.

- If x is a finite value that cannot be represented in the longlong type, a domain error occurs. In this case, the return value is 0.

- If x is a NaN or ±∞, a domain error occurs. In this case, the return value is 0.

log1p function group

The argument is x. If x satisfies x < -1, a domain error occurs. In this case, the return value is a NaN.

lrint function group

The argument is x.

- If x is a finite value that cannot be represented in the long type, a domain error occurs. In this case, the return value is 0.

- If x is a NaN or ±∞, a domain error occurs. In this case, the return value is 0.

lround function group

The argument is x.

- If x is a finite value that cannot be represented in the long type, a domain error occurs. In this case, the return value is 0.

- If x is a NaN or ±∞, a domain error occurs. In this case, the return value is 0.

remquo function group

The first argument is x1, the second argument is x2, and the third argument is x3.

- If x1 is ±∞ and x2 is not a NaN, a domain error occurs. In this case, the return value is a NaN. Note that x3 points to 0.

- If x1 is not a NaN and x2 is 0, a domain error occurs. In this case, the return value is a NaN. Note that x3 points to 0.

tgamma function group

The argument is x. If x is -∞ or a negative integer, a domain error occurs. In this case, the return value is a NaN.

carg function group

The argument is x. If the real part and imaginary part of x are 0, a domain error occurs. In this case, the return value is a NaN.

ccos function group

The argument is x.

- If the real part of x is ±∞ and the imaginary part of x is 0, a domain error occurs. In this case, the return value is NaN + 0 × i.

- If the real part of x is ±∞ and the imaginary part of x is ±∞, a domain error occurs. In this case, the return value is ∞ + NaN × i.

- If the real part of x is ±∞ and the imaginary part of x is a finite value, a domain error occurs. In this case, the return value is NaN + NaN × i.

clog function group

The argument is x. If the real part of x is ±∞ and the imaginary part of x is ±∞, a domain error occurs. In this case, the return value is ±∞ + NaN × i.

cpow function group

The first argument is x1 and the second argument is x2.

- If the imaginary part of x1 is 0 and, as a result of multiplying x2 by the real part of x1, the real part is +∞ and the imaginary part is ±∞, a domain error occurs. In this case, the return value is +∞ + NaN × i.

- If the imaginary part of x1 is 0 and, as a result of multiplying x2 by the real part of x1, the real part is a finite value and the imaginary part is ±∞, a domain error occurs. In this case, the return value is NaN + NaN × i.

- If the real part of x1 or x2 is a NaN and the imaginary parts of x1 and x2 are 0, a domain error occurs. In this case, the return value is NaN + 0 × i.

- If the real part of x1 is 0, the real part of x2 is 0 or smaller, and the imaginary parts of x1 and x2 are 0, a domain error occurs. In this case, the return value is NaN + 0 × i.

- If the real part of x1 is a negative number, the real part of x2 is a noninteger, and the imaginary parts of x1 and x2 are 0, a domain error occurs. In this case, the return value is NaN + 0 × i.

remainder function group

The first argument is x1 and the second argument is x2.

- If x1 is ±∞ and x2 is not a NaN, a domain error occurs. In this case, the return value is a NaN.

- If x1 is not a NaN and x2 is 0, a domain error occurs. In this case, the return value is a NaN.

acos function group

The argument is x.

- If x satisfies x < -1 or 1 < x, a domain error occurs. In this case, the return value is a NaN.

- If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

asin function group

The argument is x.

- If x satisfies x < -1 or 1 < x, a domain error occurs. In this case, the return value is a NaN.

- If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

atan function group

The argument is x. If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

cosh function group

The argument is x. If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

exp function group

The argument is x. If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

frexp function group

The first argument is x1 and the second argument is x2. If x1 is a NaN, a domain error occurs. In this case, the return value is a NaN. Note that the pointing target of x2 does not change.

log10 function group

The argument is x.

- If x < 0 is true, a domain error occurs. In this case, the return value is a NaN.

- If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

log function group

The argument is x.

- If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

- If x < 0 is true, a domain error occurs. In this case, the return value is a NaN.

sin function group

The argument is x. If x is ±∞ or NaN, a domain error occurs. In this case, the return value is a NaN.

cos function group

The argument is x. If x is ±∞ or NaN, a domain error occurs. In this case, the return value is a NaN.

sinh function group

The argument is x. If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

tan function group

The argument is x. If x is ±∞ or NaN, a domain error occurs. In this case, the return value is a NaN.

tanh function group

The argument is x. If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

atan2 function group

The first argument is x1 and the second argument is x2.

- If x1 and x2 are 0, a domain error occurs. In this case, the return value is a NaN.

- If x1 or x2 is a NaN, a domain error occurs. In this case, the return value is a NaN.

- If x1 and X2 are ±∞, a domain error occurs. In this case, the return value is a NaN.

ceil function group

The argument is x. If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

floor function group

The argument is x. If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

fmod function group

The first argument is x1 and the second argument is x2.

- If x2 is 0, a domain error occurs. In this case, the return value is a NaN.

- If x1 or x2 is a NaN, a domain error occurs. In this case, the return value is a NaN.

- If x1 is ±∞, a domain error occurs. In this case, the return value is a NaN.

ldexp function group

The first argument is x1 and the second argument is x2. If x1 is a NaN, a domain error occurs. In this case, the return value is a NaN.

modf function group

The first argument is x1 and the second argument is x2. If x1 is a NaN, a domain error occurs. In this case, the return value is a NaN. Note that x2 points to the NaN.

pow function group

The first argument is x1 and the second argument is x2.

- If x1 or x2 is a NaN, a domain error occurs. In this case, the return value is a NaN.

- If x1 is 0 and x2 is 0 or smaller, a domain error occurs. In this case, the return value is a NaN.

- If x1 satisfies x1 < 0 and x2 is not an integer, a domain error occurs. In this case, the return value is a NaN.

sqrt function group

The argument is x.

- If x satisfies x < 0, a domain error occurs. In this case, the return value is a NaN.

- If x is a NaN, a domain error occurs. In this case, the return value is a NaN.

(73)

The values returned by the mathematics functions on underflow range errors, whether errno is set to the value of the macro ERANGE when the integer expression math_errhandling & MATH_ERRNO is nonzero, and whether the "underflow" floating-point exception is raised when the integer expression math_errhandling & MATH_ERREXCEPT is nonzero. (7.12.1).

The return value is 0. ERANGE is set in errno in case of an underflow. An "underflow" floating-point exception is generated.

(74)

Whether a domain error occurs or zero is returned when an fmod function has a second argument of zero (7.12.10.1).

A domain error is generated. For details, see the description about the fmod function group.

(75)

The base-2 logarithm of the modulus used by the remquo functions in reducing the quotient (7.12.10.3).

31.

(76)

Whether the equivalent of signal(sig, SIG_DFL); is executed prior to the call of a signal handler, and, if not, the blocking of signals that is performed (7.14.1.1).

The signal handling functions are not supported.

(77)

The null pointer constant to which the macro NULL expands (7.17).

0.

(78)

Whether the last line of a text stream requires a terminating new-line character (7.19.2).

As per low-level interface routine specifications.

(79)

Whether space characters that are written out to a text stream immediately before a new-line character appear when read in (7.19.2).

As per low-level interface routine specifications.

(80)

The number of null characters that may be appended to data written to a binary stream (7.19.2).

As per low-level interface routine specifications.

(81)

Whether the file position indicator of an append-mode stream is initially positioned at the beginning or end of the file (7.19.3).

As per low-level interface routine specifications.

(82)

Whether a write on a text stream causes the associated file to be truncated beyond that point (7.19.3).

As per low-level interface routine specifications.

(83)

The characteristics of file buffering (7.19.3).

As per low-level interface routine specifications.

(84)

Whether a zero-length file actually exists (7.19.3).

As per low-level interface routine specifications.

(85)

The rules for composing valid file names (7.19.3).

As per low-level interface routine specifications.

(86)

Whether the same file can be simultaneously open multiple times (7.19.3).

As per low-level interface routine specifications.

(87)

The nature and choice of encodings used for multibyte characters in files (7.19.3).

The shift state is not supported as the representation form of multibyte characters.

(88)

The effect of the remove function on an open file (7.19.4.1).

The remove function is not supported.

(89)

The effect if a file with the new name exists prior to a call to the rename function (7.19.4.2).

The rename function is not supported.

(90)

Whether an open temporary file is removed upon abnormal program termination (7.19.4.3).

The tmpfile function is not supported.

(91)

Which changes of mode are permitted (if any), and under what circumstances (7.19.5.4).

If filename is a null pointer, it changes the mode of the current stream to the specified mode.

(92)

The style used to print an infinity or NaN, and the meaning of any n-char or n-wchar sequence printed for a NaN (7.19.6.1, 7.24.2.1).

++++++ is output for the positive infinity, ------ for a negative infinity, and ****** for a NaN.

n character strings or n wide character strings are not supported when a NaN is written.

(93)

The output for %p conversion in the fprintf or fwprintf function (7.19.6.1, 7.24.2.1).

Hexadecimal notation.

(94)

The interpretation of a - character that is neither the first nor the last character, nor the second where a ^ character is the first, in the scanlist for %[ conversion in the fscanf() or fwscanf() function (7.19.6.2, 7.24.2.1).

Indicates a range between the previous character and the next character.

(95)

The set of sequences matched by a %p conversion and the interpretation of the corresponding input item in the fscanf() or fwscanf() function (7.19.6.2, 7.24.2.2).

Hexadecimal number.

(96)

The value to which the macro errno is set by the fgetpos, fsetpos, or ftell functions on failure (7.19.9.1, 7.19.9.3, 7.19.9.4).

The ftell function conforms with the low-level interface routine specifications.

The fgetpos and fsetpos functions are not supported.

(97)

The meaning of any n-char or n-wchar sequence in a string representing a NaN that is converted by the strtod(), strtof(), strtold(), wcstod(), wcstof(), or wcstold() function (7.20.1.3, 7.24.4.1.1).

Interpreted as qNaN in case of the strtof, strtold, wcstod, wcstof, or wcstold function. Interpreted as a value other than a number of floating-point type in case of the strtod function.

(98)

Whether or not the strtod, strtof, strtold, wcstod, wcstof, or wcstold function sets errno to ERANGE when underflow occurs (7.20.1.3, 7.24.4.1.1).

The strtod, strtof, strtold, wcstod, wcstof and wcstold functions set ERANGE in global variable errno.

(99)

Whether the calloc, malloc, and realloc functions return a null pointer or a pointer to an allocated object when the size requested is zero (7.20.3).

NULL is returned.

(100)

Whether open streams with unwritten buffered data are flushed, open streams are closed, or temporary files are removed when the abort or _Exit function is called (7.20.4.1, 7.20.4.4).

As per low-level interface routine specifications.

(101)

The termination status returned to the host environment by the abort, exit, or _Exit function (7.20.4.1, 7.20.4.3, 7.20.4.4).

The abort, exit and _Exit functions are not supported.

(102)

The value returned by the system function when its argument is not a null pointer (7.20.4.6).

The system function is not supported.

(103)

The local time zone and Daylight Saving Time (7.23.1).

Functions that handle local time zone and Daylight Saving Time are not supported.

(104)

The range and precision of times representable in clock_t and time_t (7.23).

clock_t should be the long type, and time_t should be the long long type.

(105)

The era for the clock function (7.23.2.1).

The clock function is not supported.

(106)

The replacement string for the %Z specifier to the strftime, and wcsftime functions in the "C" locale (7.23.3.5, 7.24.5.1).

The strftime function and wcsftime function are not supported.

(107)

Whether or when the trigonometric, hyperbolic, base-e exponential, base-e logarithmic, error, and log gamma functions raise the "inexact" floating-point exception in an IEC 60559 conformant implementation (F.9).

An "inexact" floating-point exception may be generated if the hypot, ldexp, lgamma, tgamma, erfc, pow, scalbln, tan, exp, or nexttoward function group resulted in an overflow or underflow.

(108)

Whether the functions in <math.h> honor the rounding direction mode in an IEC 60559 conformant implementation (F.9).

The lround function group may not follow the rounding direction mode.

(109)

The values or expressions assigned to the macros specified in the headers <float.h>, <limits.h>, and <stdint.h> (5.2.4.2, 7.18.2, 7.18.3).

Refer to each header and file in "7. LIBRARY FUNCTIONAL SPECIFICATION".

(110)

The number, order, and encoding of bytes in any object (when not explicitly specified in this International Standard) (6.2.6.1).

Refer to "4.1.5 Internal Data Representation and Areas".

(111)

The value of the result of the sizeof operator (6.5.3.4).

Refer to "4.1.5 Internal Data Representation and Areas".

 

Translation limits

The table below shows the translation limits of CC-RX.

The upper limit depends on the memory situation of the host environment for the item "No limit".

Item

Limit

Number of nesting levels of blocks

No limit

Number of nesting levels of conditional inclusion

No limit

Number of pointers, arrays, and function declarators (in any combinations) qualifying an arithmetic, structure, union, or incomplete type in a declaration

128

Number of nesting levels of parenthesized declarators within a full declarator

No limit

Number of nesting levels of parenthesized expressions within a full expression

No limit

Number of significant initial characters in an internal identifier or a macro name

No limit

Number of significant initial characters in an external identifier

No limit

Number of external identifiers in one translation unit

No limit

Number of identifiers with block scope declared in one block

No limit

Number of macro identifiers simultaneously defined in one preprocessing translation unit

No limit

Number of parameters in one function definition

No limit

Number of arguments in one function call

No limit

Number of parameters in one macro definition

No limit

Number of arguments in one macro invocation

No limit

Number of characters in a logical source line

No limit

Number of characters in a character string literal or wide string literal (after concatenation)

No limit

Number of bytes in an object (in a hosted environment only)

2147483647

Number of nesting levels for #included files

No limit

Number of case labels for a switch statement (excluding those for any nested switch statements)

2147483647

Number of members in a single structure or union

No limit

Number of enumeration constants in a single enumeration

No limit

Number of levels of nested structure or union definitions in a single struct-declaration-list

No limit