Everything
7.6 Unsupported Libraries

Table 7.16 lists the libraries which are specified in the C language specifications but not supported by this compiler.

Table 7.16

Unsupported Libraries

No.

Header File

Library Names

1

locale.h*1

setlocale, localeconv

2

signal.h*1

signal, raise

3

stdio.h

remove, rename, tmpfile, tmpnam, fgetpos, fsetpos

4

stdlib.h

abort, atexit, exit, _Exit, getenv, system, mblen, mbtowc, wctomb, mbstowcs, wcstombs

5

string.h

strcoll, strxfrm

6

time.h

clock, difftime, mktime, time, asctime, ctime, gmtime, localtime, strftime

7

wctype.h

iswalnum, iswalpha, iswblank, iswcntrl, iswdigit, iswgraph, iswlower, iswprint, iswpunct, iswspace, iswupper, iswxdigit, iswctype, wctype, towlower, towupper, towctrans, wctrans

8

wchar.h

wcsftime, wcscoll, wcsxfrm, wctob, mbrtowc, wcrtomb, mbsrtowcs, wcsrtombs

Note 1.

The header file is not supported.