This panel is used to debug RL78 SNOOZE mode sequencer (SMS).
This panel is available only when a debug tool (simulator) that supports RL78 SMS simulation is connected.
This panel can be zoomed in and out by |
This section describes the following.
Each row corresponds to SMSIp(p:0–31).
Displays the disassembly address for each line (the value of “p” in SMSIp, ranging from 0 to 31).
It also displays a marker
indicating the next execution location (SMSS.SMSCV[4:0] (0–31)).
Displays the code for SMSIp (p:0–31) in 4-digit hexadecimal notation and in disassembled form.
HighlightsNote the line of the next command to be executed.
The highlighting color depends on the configuration in the [General - Font and Color] category of the Option dialog box. |
|
Acquires the latest data from the debug tool, and updates the contents of this panel. |
|
|
Forcibly starts SMS debugging while waiting for the SMS activation trigger. |
|
The status of the SMS is indicated by the following icons and texts.
When SMS is operating, the SMS debugging status is indicated by the following icons and texts.
in the tool bar, or by moving the mouse wheel forward or backward while holding down the [Ctrl] key.
OFF
DISABLE
STOP
TERMINATE
OPERATING
BREAK
RUN
STEP