Everything
2.12.6.1 Change display mode

Display mode can be changed to the purpose when clicking the buttons below in the toolbar.

Note that these buttons are disabled while the tracer is running.

Table 2.16

Display Modes of Trace Panel

Button

Display Mode

Displayed Content

 

Mixed display mode

Displays the instruction (disassemble results), labels, source text (corresponding source line), point trace results [IECUBE][Simulator], reset causes [IECUBE], and break causes (default).

 

Disassemble display mode

Displays the instruction (disassemble results), labels, point trace results [IECUBE][Simulator], reset causes [IECUBE], and break causes.

 

Source display mode

Displays the source text (corresponding source line), reset causes [IECUBE], and break causes.

However, when a place where no debugging information is present is executed, "<No Debug Information>" is displayed.

Figure 2.81

Example of Source Display Mode View (Trace Panel)