Everything
 

Pull up/Pull down dialog box


This dialog box is used to set or change the pin connection information of the pull-up/pull-down resistors, which are one of the connection parts of the I/O Panel window.

The setting method for these connection parts differs from those for other parts. The connection information of all the pins is managed as a group in this dialog box.

Figure A.89

Pull up/Pull down Dialog Box

 

This section describes the following.

[How to open]

-

With the I/O Panel window in focus, click the button or select [Pull up/Pull down...] from the [Parts] menu.

[Description of each area]

(1)

Connection information display area

Pin name

Displays the names of the pins that can be connected to pull-up/pull-down resistors.

Pull Up/Pull Down

Displays the connected status of the pins.

Pull Up

Indicates pull-up resistor is connected.

Pull Down

Indicates pull-down resistor connected.

-

Indicates no pull-up/pull-down resistor connected.

Buttons

Changes the pin connection information of the pull-up/pull-down resistors.

Pull Up

Connects the pins selected to pull-up resistors.

When connection is completed, "Pull Up" is displayed.

Pull Down

Connects the pins selected to pull-down resistors.

When connection is completed, "Pull Down" is displayed.

Disconnect

Cancels the connected status of the pins selected.

When connection is completed, "-" is displayed.

[Function buttons]

Button

Function

OK

Validates the settings and closes this dialog box.

Cancel

Cancels the settings and closes this dialog box.