Everything

PseudoErrorInfo


This class holds ECM error information (return value of the debugger.PseudoError.Get function). [RH850][E1/E2/E2 Lite/E20/Full-spec emulator/IE850A]

[Type]

class PseudoErrorInfo:
        Number = ""
        Name = ""
        BitName = ""
        Category = ""
        Error = False

[Variable]

Variable

Description

Number

This holds the error number.

Name

This holds the name (abbreviated form) of the ECM error.

BitName

This holds the name of the IOR bit.

Category

This holds the category name.

Error

This holds information on whether an error was generated.

True: An error was generated.

False: An error was not generated.

[Detailed description]

Example 1.

"PseudoErrorInfo" is a class, and it is passed as the return value when the debugger.PseudoError.Get function is executed.