Everything

debugger.Performance.Enable


This function enables performance measurement. [RH850][E1/E2/E2 Lite/E20/Full-spec emulator/IE850A]

[Specification format]

debugger.Performance.Enable(performanceNumber = "")

[Argument(s)]

Argument

Description

performanceNumber

Specify the performance measurement event number to enable.

[Return value]

If performance measurement was enabled successfully: True

If there was an error when enabling performance measurement: False

[Detailed description]

-

This function enables performance measurement of a performance measurement event number specified by performanceNumber.

-

If performanceNumber is not specified, then performance measurement of all performance measurement event numbers will be enabled.

[Example of use]

>>>debugger.Performance.Enable()
True
>>>