Everything

debugger.Performance.Information


This function displays performance measurement information. [RH850][E1/E2/E2 Lite/E20/Full-spec emulator/IE850A]

[Specification format]

debugger.Performance.Information()

[Argument(s)]

None

[Return value]

List of performance measurement information (see the PerformanceEventInfo class for detail)

[Detailed description]

-

This function displays software trace information displays in the following format.

[performance-measurement-event-number] [performance-measurement-name] [state] [start-address] - [end-address]

[Example of use]

>>>pi = debugger.Performance.Information()
1 PythonPerformanceMeasurement001 Enable 0x00000200 - 0x00000300
>>>print pi.Enable
True
>>>print pi.StartAddress
0x00000200
>>>