Everything

csplus.skip_all_breakpoints


This function skips all breakpoints.

[Specification format]

csplus.skip_all_breakpoints(skip=True)

[Argument(s)]

Argument

Description

skip

Specify whether all breakpoints in the current workspace should be skipped

[Return value]

None

[Detailed description]

-

This command just ignore all breakpoints when running without changing the enabled state of breakpoints.

[Example of use]

>>> csplus.skip_all_breakpoints(True)
>>> csplus.resume_debug_session(0)