2.3 Control CS+ in the Python 3 Execution Environment
CS+ can be controlled by scripts for Python 3. This section describes how to control CS+ from the command prompt.
(1) | Start up the server for the external communications facility in the Python console of CS+. |
>> server.Start()
(2) | Run Python from the command prompt. |
(3) | Add the integration_service folder to the settings for paths. |
(4) | Import a csplus module by using an import statement. |
(5) | Call the functions of the csplus module to control CS+. Start by calling the connect() function. To close the server, call the disconnect() function or terminate() function. |
>>> import sys
>>> sys.path.append("C:\Program Files (x86)\Renesas Electronics\CS+\CC\Plugins\PythonConsole\integration_service")
>>> import csplus
>>> csplus.connect()
>>> session_id = csplus.launch_debug_session("")
>>>
|
For details on the functions of the csplus module, see “C. External Communications with the Python 3 Execution Environment/csplus Module Functions”.