1.4 Operating Environment
Below are the system requirements for this product.
Processor and main memory that can comfortably run the software described in the software environment
Display: Resolution at least 1,024 x 768 (recommended 1920 x 1080)
Interface: USB 2.0
- | Microsoft .NET Framework 4.8 |
- | Microsoft Visual C++ 2015-2022 Redistributable (x86) |
- | Microsoft Edge WebView2 Runtime |
- | Online help: Edge, Chrome, or Firefox (The latest version is recommended) |
(3) | Supported target environments |
- | Full-spec emulator [RH850] |
- | E2 emulator [RH850][RX][RL78] |
- | E2 emulator Lite [RH850][RX][RL78] |