Everything

Open dialog box

This dialog box reads the analysis information saved as task analyzer trace data and displays the information in the Child-panel display area on the Realtime OS Task Analyzer panel.
Figure A-10. Open Dialog Box
The following items are explained here.
[How to open]
- Select [Opens trace data...] from the menu list located on the Toolbar on the Realtime OS Task Analyzer panel.
[Description of each area]
(1) [Look in]
Selects a folder containing the task analyzer trace data.
(2) List of files
Lists the files that meet the conditions selected in [Look in] and [Files of type].
(3) [File name]
Specifies the name of the file containing the task analyzer trace data to be read.
(4) [Files of type]
Selects "Task analyzer trace data (*.tad)" as the type of the file to be read.
[Function buttons]
Button
Function
Open
From the folder specified in [Look in], read the file specified in [File name] and [Files of type] to display the applicable information on the Analysis Result panel.
Cancel
Ignores the setting and closes this dialog box.