Everything

Analysis Result panel


This panel is a Child-panel display area of the Realtime OS Task Analyzer panel to display the analysis information such as execution transition state of the processing program, the state of real-time OS resource usage, and the CPU usage status.

Figure A.2

Analysis Result Panel

 

The following items are explained here.

[How to open]

-

Press the button located on the Toolbar on the Realtime OS Task Analyzer panel.

[Description of each area]

(1)

Toolbar

This area consists of the following buttons.

 

In the Analysis information diagram area, changes the red-highlighted processing interval from "the processing interval now being highlighted in red" to "the processing interval which was executed prior to the highlighted processing interval".

 

In the Analysis information diagram area, changes the red-highlighted processing interval from "the interval now being highlighted in red" to "the interval which was executed immediately after the highlighted processing interval".

 

In the Analysis information diagram area, changes the red-highlighted processing interval from "the interval now being highlighted in red" to "the interval at which the given processing program was executed first".

Note that the "first executed" processing interval is the interval at which the given processing program was executed first during trace data acquisition.

 

In the Analysis information diagram area, changes the red-highlighted processing interval from "the interval now being highlighted in red" to "the interval just before which the given processing program was executed".

 

In the Analysis information diagram area, changes the red-highlighted processing interval from "the interval now being highlighted in red" to "the interval immediately after which the given processing program was executed".

 

In the Analysis information diagram area, changes the red-highlighted processing interval from "the interval now being highlighted in red" to "the interval at which the given processing program was executed last".

Note that the "last executed processing interval" is the interval at which the processing program was executed last during trace data acquisition.

 

Opens the Chart Visualization Chooser dialog box to specify the type of state line to be displayed as an execution transition state of the processing program, and whether an event mark is or is not displayed as real-time OS resources usage status, in the Analysis information diagram area.

 

(2)

Analysis information display area

Displays analysis information including the execution transition state of the processing program, the state of real-time OS resource usage, and the CPU usage status, among the acquired trace data.

(a)

Analysis information table area

Displays the analysis information about the CPU usage status in table form.

Figure A.3

Analysis Information Table Area

 

The following table shows the elements which make up this area.

The analysis information displayed in this area is the CPU usage status during trace data acquisition or during the Analysis information extraction interval during which data is extracted by mouse cursor drag & drop in the Execution transition display area in the Analysis information diagram area.

 

Opens the Column Chooser dialog box to specify the types of items to be displayed as the CPU usage status in the Analysis information table area.

/

Displays the sort order in the target column.

 

Indicates the sort in ascending order.

 

Indicates the sort in descending order.

/

Displays whether a filter condition is or is not set for the target column.

 

Indicates that a filter condition is not set for the column.

Clicking on this icon displays the following filtering menu.

(All)

Displays all analysis information.

(Custom)

Opens the Filter Settings dialog box to set a filter condition on analysis information which is displayed as CPU usage status.

(Blanks)

Only displays the lines indicated by "-".

(NonBlanks)

Displays lines other than those indicated by "-".

Object of display

Only displays the target object lines.

 

Indicates a column for which a filter condition has been set.

/

Indicates whether the target column is or is not the scroll target during horizontal scrolling using the scroll bar.

 

Indicates that the column is the scroll target.

 

Indicates that the column is not the scroll target.

Category

Displays the type of the objects (processing program or real-time OS resource).

Note that the processing programs displayed in this column are limited to the ones which were executed during trace data acquisition, and the real-time OS resource displayed in the column is limited to the one whose task was queued in the task wait queue of the object during trace data acquisition.

Name

Displays the ID name of the object.

ID

Displays the ID number of the object.

PE Number

Always displays "-".

CPU Usage Rate

Displays the execution ratio (total ratio or user/kernel ratio) for the processing program. The [Context menu] menu is used to switch between "total ratio" and "user/kernel ratio".

Total Execution Time

Displays the total execution time of the processing program.

Average Execution Time

Displays the average continuous execution time of the processing program.

Maximum Execution Time

Displays the maximum continuous execution time of the processing program.

Minimum Execution Time

Displays the minimum continuous execution time of the processing program.

Execution Count

Displays the execution count (number of times of execution from the start) of the processing program.

 

(b)

Analysis information diagram area

Displays analysis information about the execution transition state of the processing program and real-time OS resource usage status in diagram form.

Figure A.4

Analysis Information Diagram Area

 

The elements which make up this area are as follows.

<1>

Start time of execution transition display

Displays start time of Execution transition display area.

<2>

End time of execution transition display

Displays end time of Execution transition display area.

<3>

Execution transition display area

Displays the execution transition state of the processing program and real-time OS resource usage status for the displaying trace data specified by Zoom in or out slider of execution transition display or Zoom in button of execution transition display and Zoom out button of execution transition display.

Period which to display in the Execution transition display area can be changed from 1us to 1ms.

 

In this area, execution transition state of the processing program is indicated as follows:

 

Indicates that a processing program was executed.

 

Indicates that a processing program has been suspended.

 

Indicates that a task is in transition to the READY state.

 

Indicates that a task is in transition to the WAITING state, or a task has been queued in the wait queue of the real-time OS resource.

 

Indicates that a task is in transition to the SUSPENDED state.

 

Indicates that a task is in transition to the WAITING-SUSPENDED state.

 

Indicates that a task is in transition to the DORMANT state.

 

Indicates that RI78V4 processing was executed in association with the issued service call.

 

When "processing program" has been selected in the Analysis information table area, this color indicates the processing interval that was executed first among the intervals shown by .

Pressing the Toolbar buttons ( , , etc.) moves to the corresponding processing interval.

 

In this area, usage status of the real-time OS resource is indicated with the event marks below:

 

Indicates that a service call has been issued.

When the mouse cursor is placed on this mark, the "service call name" (ID number of the object) for which a service call is issued.

 

Indicates that a service call has been terminated normally.

When the mouse cursor is placed on this mark, "E_OK (0)" appears indicating normal termination of the service call.

 

Indicates that a service call has been terminated abnormally.

When the mouse cursor is placed on this mark, "macro name (value)" appears indicating abnormal termination of the service call.

 

Indicates that a service call has been timed out.

When the mouse cursor is placed on this mark, "E_TMOUT (-50)" appears indicating timeout of the service call.

Remark

By dragging and dropping the mouse cursor in this area, the analysis information to be displayed in the Analysis information table area can be updated from "analysis information during the trace data acquisition period" to "analysis information during the analysis information extraction interval".

To cancel "analysis information during the analysis information extraction interval," move the mouse cursor to within the Analysis information diagram area, and then double click on the left mouse button while pressing the [Ctrl] key.
For details on this operation, see section "2.4.6 Limiting range of usage status".

<4>

Scroll bar of execution transition display

Specifies the period at which information is displayed in the Execution transition display area during the trace data acquisition period.

Left end of scroll bar is start position of trace data acquisition period. Right end of scroll bar is end position of trace data acquisition period.

<5>

Zoom in or out slider of execution transition display

Specifies to zoom in or out Execution transition display area.

When you drag slider to right, execution transition display area is zoomed in and when you drag slider to

left, execution transition display area is zoomed out.

<6>

Zoom in button of execution transition display

To press the button, Execution transition display area is zoomed in.

Displaying diagram is zoomed in and interval from Start time of execution transition display and End time of execution transition display become shorter.

<7>

Zoom out button of execution transition display

To press the button, Execution transition display area is zoomed out.

Displaying diagram is zoomed out and interval from Start time of execution transition display and End time of execution transition display become longer.

Remark

By using the mouse wheel with the [Ctrl] key pressed, the display within the Execution transition display area can be zoomed in or out.

Figure A.5

Extraction of Analysis Information

 

Elements which make up the analysis information extraction interval are as follows:

<a>

Start time of analysis information extraction

Displays the "time when trace data acquisition has been started" during the Analysis information extraction interval.

The Analysis information extraction interval can be changed by scrolling the mark right under the extraction start time, in the same way as with the usual scroll bar.

<b>

End time of analysis information extraction

Displays the "time when trace data acquisition has been finished" during the Analysis information extraction interval.

The Analysis information extraction interval can be changed by scrolling the mark right under the extraction end time, in the same way as with the usual scroll bar.

<c>

Analysis information extraction interval

Displays the execution transition state of the processing program and the real-time OS resource usage status during the Analysis information extraction interval.

The Analysis information extraction interval appears in magenta background.

(3)

Analysis information overview display area

This area is displayed overview as an execution transition state of the processing program wider than Execution transition display area in diagram form.

Figure A.6

Analysis information overview display area

 

<1>

Start time of overview display

Displays start time of Overview display area.

<2>

End time of overview display

Displays end time of Overview display area.

<3>

Overview display area

Displays the overview as an execution transition state of the processing program and real-time OS resource usage status for the displaying trace data specified by Zoom in or out slider of overview display or Zoom in button of overview display and Zoom out button of overview display.

Period which to display in the Overview display area can be changed from 1us to 100ms.

<4>

Execution transition display control

Displays the period at which information is displayed in the Execution transition display area during the trace data acquisition period.

In addition, by scrolling this control, in the Execution transition display area can be changed in the same way as with the usual scroll bar.

<5>

Scroll bar of overview display

Specifies the period at which information is displayed in the Overview display area during the trace data acquisition period.

Left end of scroll bar is start position of trace data acquisition period. Right end of scroll bar is end position of trace data acquisition period.

<6>

Zoom in or out slider of overview display

Specifies to zoom in or out Overview display area.

When you drag slider to right, overview display area is zoomed in and when you drag slider to left, overview display area is zoomed out.

<7>

Zoom in button of overview display

To press the button, Overview display area is zoomed in.

Displaying diagram is zoomed in and interval from Start time of overview display and End time of overview display become shorter.

<8>

Zoom out button of overview display

To press the button, Overview display area is zoomed out.

Displaying diagram is zoomed out and interval from Start time of overview display and End time of overview display become longer.

Remark

By using the mouse wheel with the [Ctrl] key pressed, the display within the Overview display area can be zoomed in or out.

[Context menu]

By right-clicking on the mouse, the following context menu is displayed:

Display Total Ratio

Switches the ratio in the CPU Usage Rate column to Total Ratio.

When this menu has been selected, "the ratio of the total execution time of the processing program to the total execution time of all the processing programs" is displayed in the CPU Usage Rate column.

Display User/Kernel Ratio

Switches the ratio in the CPU Usage Rate column to User/Kernel Ratio.

When this menu has been selected, "the ratio of the total execution time of the processing program to the total execution time of all the processing programs" is displayed in the CPU Usage Rate column in the following form:

xxx / yyy

-

xxx

The ratio of the total execution time of the given processing program (excluding RI78V4 processing time associated with service call issuance) to the total execution time of all the processing programs.

-

yyy

The ratio of the RI78V4 total processing time associated with service call issuance in the given processing program to the total execution time of all the processing programs.

Jump to Source

Opens the Editor panel and displays the source of the processing program.

Jump to Disassemble

Opens the Disassemble panel and displays the disassemble results of the processing program.

Go to Maximum Execution Time

Highlights in red the portion representing the maximum continuous execution time of the processing program in the Analysis information diagram area.

Go to Minimum Execution Time

Highlights in red the portion representing the minimum continuous execution time of the processing program in the Analysis information diagram area.