3.5  When the Panel Is Opened during Execution of Program
 
The updated static analysis information will be displayed.  The dynamic analysis information is not updated. 
-  | If this panel has been never opened since CS+ was launched:  | 
 
-  | If this panel has been opened once since CS+ was launched:  | 
 
-  | If this panel has been never opened since CS+ was launched: 
The updated static analysis information will be displayed.  The dynamic analysis information is not updated.  
  | 
 
-  | If this panel has been opened once since CS+ was launched: 
The previous display contents will be displayed.   | 
 
The updated static analysis information will be displayed.  The dynamic analysis information is not updated. 
The previous display contents will be displayed.