Select the build tool node on the project tree and select the [Compile Options] tab on the Property panel.
To perform optimization with the execution speed precedence, select [Speed precedence(-Ospeed)] in the [Optimization Level] property in the [Optimization] category.
![](Build-RH850_Eng-20.gif)
You can also set the option in the same way with the [Optimization Level] property in the [Frequently Used Options(for Compile)] category on the [Common Options] tab. |